2025-01-27 10:48 AM - last edited on 2025-01-28 12:30 PM by mƎALLEm
Hi to All
I would like to try a configuration for GPDMA1 for STM32H503CBU6 using memory to memory. I will would like to use a Link-Lists. Source will be two different array of DATA Bytes inside the Flash Memory and Destination will be the GPIOB. It will be circular mode just to try out the configuration. Is this possible?
If possible, what settings will be there for GPDMA1_CxCR, GPDMA1_CxTR1,GPDMA1_CxTR2, GPDMA1_CxBR1, GPDMA1_CxSAR, GPDMA1_CxDAR, GPDMA1_CxTR3, GPDMA1_CxBR2 and GPDMA1_CxLLR?
I have read the manual regarding memory to memory but i'm not satisfied with the explanation. Maybe someone out there would be kind enough to share some knowledge.
thanks and best regards
2025-01-29 2:28 AM
Hello @Rashid,
Besides the RM, there is an application note on How to use the GPDMA for STM32, covering STM32H5 product, check section "GPDMA configuration for internal memories".
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.