2025-07-31 3:41 PM
In developing a bootloader and application for an STM32H5 project using STM32CubeIDE v1.19.0, and STM32H5xx HAL Driver v1.5.0.RC1; when I place the ISR at 0x08008200, I can start the debug process but the application appears to be stuck in void SVC_Handler(void) once an interrupt occurs.
What's interesting is that if I adjust the ISR location to 0x08008000, or 0x08008400, and define VECT_TAB_OFFSET in system_stm32h5xx.c [along with changing definition of .isr_vector to 0x08008000/0x08008400 in LinkerScript.ld] everything behaves as expected; it's only when setting to 0x08008200 that things break.
I previously had a build environment with STM32CubeIDE v1.15.1 using v1.4.0 STM32Cube MCU package and everything worked fine then.
Any guidance on where to look to zero-in on what might be the culprit?
Solved! Go to Solution.
2025-07-31 3:46 PM - edited 2025-07-31 3:47 PM
The vector table is over 512 bytes but below/at 1024 bytes, so must be aligned to a 1024-byte boundary. 1024 = 0x400.
This is a Cortex restriction.
2025-07-31 3:46 PM - edited 2025-07-31 3:47 PM
The vector table is over 512 bytes but below/at 1024 bytes, so must be aligned to a 1024-byte boundary. 1024 = 0x400.
This is a Cortex restriction.
2025-07-31 4:03 PM
Ah, ok. That would certainly explain things. Thank you!
2025-07-31 6:23 PM
I suspect that if you write a value to SCB->VTOR the low order bits will be STZ (stuck-at-zero)
The size of the customer (ST) vector/interrupt table gets baked into the core, and drives the alignment.
2025-08-01 1:01 AM - edited 2025-08-01 1:07 AM
> SCB->VTOR the low order bits will be STZ (stuck-at-zero)
When we discussed this back then, I tried, and they weren't. Instead, the behaviour is, that the processor doesn't ADD the vector offset to VTOR when invoked, instead it ORs it.
It's a detail irrelevant to the rule as the consequence is exactly the same, I just found it amusing.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.