2021-09-03 1:07 AM
Hi,
I have a new project with STM32G474CE and cant get it start. If I program it with STM32CubeProgrammer it runs the a simple code for led blinking. I checked all VDD,Vref,Vbat pins and all okay. But after powering it off and on again, code gets stuck.
I debug it with keil and see it is stuck in some loop at the beginning. Same thing happens if I programm it with keil, it cant reach to led blinking.
I checked the option bits with STM32CubeProgrammer for boot0 and it is unchecked.
Solved! Go to Solution.
2021-09-03 2:21 AM
Sorry. Just figured it out. It is on system memory. Boot conf. is not correct. It is solved.
2021-09-03 2:21 AM
Sorry. Just figured it out. It is on system memory. Boot conf. is not correct. It is solved.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.