2021-03-26 4:39 AM
Hello All,
I am trying to send some classic CAN messages via the FDCAN3 module on STM32G474CE device. I have only pins for FDCAN3 free. My FDCAN clock is PCLK1 with a frequency of 64MHz.
When I try to transmit a CAN message, firstly there is no transmission on the line (as seen from the oscilloscope and PCAN-Explorer software.
My questions are: 1. Can I even use FDCAN3 alone to transmit messages? Is it necessary to enable FDCAN1 for it or something?
Here is how CubeMX has programmed the configuration registers
hfdcan3.Instance = FDCAN3;
hfdcan3.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
hfdcan3.Init.Mode = FDCAN_MODE_NORMAL;
hfdcan3.Init.AutoRetransmission = DISABLE;
hfdcan3.Init.TransmitPause = DISABLE;
hfdcan3.Init.ProtocolException = DISABLE;
hfdcan3.Init.NominalPrescaler = 16;
hfdcan3.Init.NominalSyncJumpWidth = 1;
hfdcan3.Init.NominalTimeSeg1 = 13;
hfdcan3.Init.NominalTimeSeg2 = 2;
hfdcan3.Init.DataPrescaler = 16;
hfdcan3.Init.DataSyncJumpWidth = 1;
hfdcan3.Init.DataTimeSeg1 = 13;
hfdcan3.Init.DataTimeSeg2 = 2;
hfdcan3.Init.StdFiltersNbr = 1;
hfdcan3.Init.ExtFiltersNbr = 0;
hfdcan3.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
if (HAL_FDCAN_Init(&hfdcan3) != HAL_OK)
{
Error_Handler();
}
Any help on this?
Solved! Go to Solution.
2021-03-26 1:46 PM
Hi,
Please see this post: https://community.st.com/s/question/0D53W0000080SyvSAE/get-no-coomunication-via-fdcan1-on-stm32g431rb-nucleo-board
Best Regards,
Slawek
2021-03-26 1:46 PM
Hi,
Please see this post: https://community.st.com/s/question/0D53W0000080SyvSAE/get-no-coomunication-via-fdcan1-on-stm32g431rb-nucleo-board
Best Regards,
Slawek
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.