2021-02-20 8:06 AM
Hi,
I would like to make a new electronic design with the STM32G473, using I2C2.
But it seems there is a mistake in the datasheet regarding the pinout.
On pin description it says:
PA8 = I2C2 SDA
PA9 = I2C2 CLK
PA10 = I2C2 SMBA
Whereas on Alternate function it says:
PA8 = I2C2 SMBA
PA9 = I2C2 CLK
PA10 = I2C2 SDA
Which one is correct?
If I look on other similar MCUs, I think the second version (Alternate function) is correct, but if I check on CubeMX, it says the same as on pin description.
Thanks for your help!
Solved! Go to Solution.
2021-02-23 3:47 AM
Hello @thomas23 ,
The pin description is the correct one:
PA8 = I2C2 SDA
PA10 = I2C2 SMBA
I will report the error to our team for correction.
Thanks for your contribution
Imen
2021-02-22 12:22 AM
Hello @thomas23,
I will check and get back to you
Imen
2021-02-22 11:03 AM
Ok thanks!
2021-02-23 3:47 AM
Hello @thomas23 ,
The pin description is the correct one:
PA8 = I2C2 SDA
PA10 = I2C2 SMBA
I will report the error to our team for correction.
Thanks for your contribution
Imen
2022-07-25 9:40 PM
This is still an issue even on the latest DS12712 rev4 datasheet available to download. Please be aware!
2023-02-08 3:28 AM
Just got bitten by this; request User Manual update please.
2023-04-24 2:16 AM
Hello,
This issue is fixed and the new Datasheet revision is published in the ST website: DS12712 Rev 5.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.