2023-07-01 3:09 PM
Hi,
as advertised
of course , but no :
- no UART4 as the datasheet , page 14/200 (false because UFQFPN48 has 4 more pins than LQFP48 ?)
- no UART4 as CubeMx : PC10 and PC11 are present , but no UART4
I have got a STM32G431CBU6 from an chinese board maker , nice board with amazing MCU
tried UART4 as STM32duino's Serial4 : it works , so USART4 is present , officially or not ...
(didn't try the handshaking lines)
Solved! Go to Solution.
2024-03-22 1:15 AM - edited 2024-03-22 1:19 AM
Hello @mwalt.3 ,
The issue is fixed in DS12589 Rev 6 and in STM32CubeMX 6.11.0.
Thank you for your contribution in STCommunity.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-07-02 12:14 AM
as page 14 shows, STM32G431CBU6 should have the uart, only in lqfp48 not.
(lqfp48 has more vdd/vss pins, so pc10/11 missing)
2023-07-02 12:44 AM
oh right , thanks , I had (don't now why) Rev 2 , but its actually Rev 6
still the issue with CubeMx
2023-07-05 7:00 AM - edited 2023-07-05 7:10 AM
Hello @mwalt.3 ,
I confirm this issue in the STM32CubeMX 6.8.1 version.
I reported this issue internally.
Internal ticket number: 146117 (This is an internal tracking number and is not accessible or usable by customers).
When your question is answered, please close this topic by choosing "Accept as Solution". This will help other users find that answer faster
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-22 1:15 AM - edited 2024-03-22 1:19 AM
Hello @mwalt.3 ,
The issue is fixed in DS12589 Rev 6 and in STM32CubeMX 6.11.0.
Thank you for your contribution in STCommunity.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.