2025-03-28 6:22 AM
Hi there,
Context
I implement a basic code where I check the reset cause flag SFTRSTF (i.e. software reset). If this flag is active, I activate the LED on (LED off otherwise).
I read out the reset cause from:
uint32_t myResetCause = RCC->CSR;
RCC->CSR |= RCC_CSR_RMVF; // Clean reset causes for next startIssue
After flashing this code, I power off my MCU and I remove the debugger cable.
Then I power on my MCU and it activates the LED, meaning the software reset has been detected, but I triggered an hardware reset ...!
Do I miss to clean another register?
Is there any information somewhere about this behavior?
Is it an expected behavior??
Solved! Go to Solution.
2025-03-28 6:27 AM
Ok my issue is related to a RAM area that I configured to be ignored by the BSS and that took random values at boot.
2025-03-28 6:27 AM
Ok my issue is related to a RAM area that I configured to be ignored by the BSS and that took random values at boot.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.