2019-07-09 10:43 PM
I am using STMG32G070RB8TX for Programming the device is detected in TS link Utility but when i compile the compiler throws an error below is the description of the error.
Error in final launch sequence:
Error in initializing ST-LINK device.
Reason: (255) Unknown. Please check power and cabling to target.
Error in initializing ST-LINK device.
Reason: Unknown. Please check power and cabling to target.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Target unknown error 19
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.