2024-03-06 3:28 AM
Hi!
I use the RTC of a STM32G030K6T. It is clocked by LSI (appr. 32kHz). And PREDIV_A is 0x0 and PREDIV_S is 0x7FFF. So I expect that RTC_SSR overflows every 1.024sec...
But: It overflows every 0.687sec... As if the LSI frequency would be 47712Hz...
I mentioned this after I soldered the positive contact of a LiFePO4 battery... Now I cannot easily disconnect power... Triggering the reset pin does not change the fast RTC... A software reset does not help, too...
How could I possibly damage the LSI by making a solder joint at the other side of the board? I even have a voltage clamp at 3.5V and a LDO (3.0V) between that solder joint and the STM32G030.
Or is it more likely that I made some last minute firmware changes? What could that be?
Thx.
Bye.
Solved! Go to Solution.
2024-03-08 3:19 AM
oh... ok... that would examine if the LSI is funny...
but: after a power cycle everything is back to normal... :grinning_face:
i think the LSI was puzzled by several power glitches during my soldering... it was quite wild... with a lot of sudden power interruptions... i have heard that power glitches can be used to get the firmware out of some Apple devices... :face_savoring_food:
2024-03-06 7:46 AM
LSI can be output to one of MCO or LSCO pins, and its frequency measured there.
JW
2024-03-08 3:14 AM
after a power cycle (after some soldering under the hood... this time i turned off the soldering iron shortly before touching the board...) the LSI ticks at appr. 31765Hz again... giggle
what might be the reason?
2024-03-08 3:19 AM
oh... ok... that would examine if the LSI is funny...
but: after a power cycle everything is back to normal... :grinning_face:
i think the LSI was puzzled by several power glitches during my soldering... it was quite wild... with a lot of sudden power interruptions... i have heard that power glitches can be used to get the firmware out of some Apple devices... :face_savoring_food:
2024-03-08 3:21 AM
Maybe this is an instance of the Unstable LSI when it clocks RTC or CSS on LSE erratum.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.