2023-01-31 1:28 AM
Hi I am using an STM32G071 Nucleo board and would like to know if it is possible to achieve the advertised current of 40nA in shutdown mode.
I have no problems entering shutdown mode but the observed current with my nRF PPK2 is closer to 1uA. I have disabled the RTC.
1) Is the current of 40nA possible on the Nucleo board?
2) Are there any required steps before entering shutdown mode?
Thank you
Solved! Go to Solution.
2023-03-16 5:23 PM
It kind of is withing the specs, but typically the devices measure to... the typical values.
Another possibility is that SWD pins could be leaking some current to/from the ST-LINK through the internal pull-up/down resistors, which are enabled by a reset.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.