2018-05-22 6:07 AM
Hello,
I can not get usart2 working in asynchronous mode on STM32f767zi-nucleo.
My clock configuration function contains
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USART2|RCC_PERIPHCLK_USART3|RCC_PERIPHCLK_CLK48;
PeriphClkInitStruct.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1;In main() I call
static void MX_USART2_UART_Init(void)
{huart2.Instance = USART2;
huart2.Init.BaudRate = 115200; huart2.Init.WordLength = /*UART_WORDLENGTH_7B*/UART_WORDLENGTH_8B; huart2.Init.StopBits = UART_STOPBITS_1; huart2.Init.Parity = UART_PARITY_NONE; huart2.Init.Mode = UART_MODE_TX_RX; huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart2.Init.OverSampling = UART_OVERSAMPLING_16; huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; if (HAL_UART_Init(&huart2) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}
When I try to send something to USART2 with HAL_UART_Transmit I get return code HAL_OK, but I can't see anything on serial port.
Can you give me an advice?
Thank you
Vaclav
2018-05-22 6:20 AM
Read back and check the relevant RCC, GPIO and UART registers.
JW
2018-05-22 6:43 AM
After trying to send a message the USART2 registers look like this:
CR1 0x0
CR2 0x0
CR3 0x0
BRR 0x0
GTPR 0x0
RTOR 0x0
RQR empty
ISR 0xc0
ICR empty
RDR 0x0
TDR 0x0
2018-05-22 9:30 AM
,
,
Looks like the clock isn't actually enabled. USART2 on PA2/PA3 would look like this in a complete form. CubeMX spreads things all over the place. Check the pin/clock stuff generated in the MSP code
void USART2_Init(void)
,
{,
, GPIO_InitTypeDef , GPIO_InitStruct,, /* ♯ ♯ -1- Enable peripherals and GPIO Clocks ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ */
,
, /* Enable GPIO TX/RX clock */,
, , ,__HAL_RCC_GPIOA_CLK_ENABLE(),,
, /* Enable USART2 clock */,
, , ,__HAL_RCC_USART2_CLK_ENABLE(),,
, , ,,
, /* ♯ ♯ -2- Configure peripheral GPIO ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ */,
, /* UART TX and RX GPIO pin configuration , */,
, GPIO_InitStruct.Pin , , , , , , = GPIO_PIN_2 | GPIO_PIN_3,,
, GPIO_InitStruct.Mode , , , , , = GPIO_MODE_AF_PP,,
, GPIO_InitStruct.Pull , , , , , = GPIO_PULLUP,,
, GPIO_InitStruct.Speed , , , , = GPIO_SPEED_FAST,,
, GPIO_InitStruct.Alternate = GPIO_AF7_USART2,, HAL_GPIO_Init(GPIOA, &,GPIO_InitStruct),
/* ♯ ♯ -1- Configure the UART peripheral ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ */
,
, /* Put the USART peripheral in the Asynchronous mode (UART Mode) */,
, /* UART configured as follows:,
, , , , , - Word Length = 8 Bits,
, , , , , - Stop Bit = One Stop bit,
, , , , , - Parity = None,
, , , , , - BaudRate = 9600 baud,
, , , , , - Hardware flow control disabled (RTS and CTS signals) */,
, UartHandle.Instance , , , , , , , = USART2,, UartHandle.Init.BaudRate , , = 115200,
,
, UartHandle.Init.WordLength = UART_WORDLENGTH_8B,,
, UartHandle.Init.StopBits , , = UART_STOPBITS_1,,
, UartHandle.Init.Parity , , , , = UART_PARITY_NONE,,
, UartHandle.Init.HwFlowCtl , = UART_HWCONTROL_NONE,,
, UartHandle.Init.Mode , , , , , , = UART_MODE_TX_RX,,
♯ ifdef UART_ADVFEATURE_NO_INIT,
, UartHandle.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT,,
♯ endif, if (HAL_UART_DeInit(&,UartHandle) != HAL_OK)
,
, {,
, , , Error_Handler(),,
, }, if (HAL_UART_Init(&,UartHandle) != HAL_OK)
,
, {,
, , , Error_Handler(),,
, }}
2018-05-22 11:26 AM
As Clive said, this indicates that the USART clock is not enabled. You should verify this by reading out the relevant RCC registers.
Blind shot: Is PeriphClkInitStruct initialized in all its elements?
JW
2018-05-23 12:11 AM
Hello, the problem was that I forgot to enable the USART clock by
__USART2_CLK_ENABLE. It works now. Thank you all.
Vaclav
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.