2017-08-24 3:20 AM
I am trying to get the STM32F767 in the LQFP100 package to go into standby but the internal 1.2v regulator stays on.
There is a complication in that it uses external oscillators while running, but for shutdown I switch to HSI, disable the external oscillator and try to enter standby. GPIOE pin 2 asserts then fades away, suggesting that standby is sort of being entered, but the 1.2V regulator stays on, pulling around 5mA. What is keeping it on?
By the way, I didn't have this problem with a previous prototype that used a crystal for the HSE, just call
HAL_PWR_EnterSTANDBYMode() and
the regulator turns off.__disable_irq();
// configure WUP4 for wakeup
//HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN4_LOW); // heh, doesn't work PWR->CR2 |= PWR_CR2_WUPP4; PWR->CSR2 &= ~PWR_CSR2_EWUP4; PWR->CR2 |= PWR_CR2_CWUPF4; PWR->CSR2 |= PWR_CSR2_EWUP4;HAL_RCC_MCOConfig(RCC_MCO1, RCC_MCO1SOURCE_HSI, RCC_MCODIV_1); // MCO1 to HSI RCC->CFGR &= ~RCC_CFGR_SW_Msk; // Select HSI for sysclk while (RCC->CFGR & RCC_CFGR_SWS); // wait until HSI selected RCC->CR &= ~RCC_CR_HSEON; // disable HSE HAL_GPIO_WritePin(GPIOA, GPIO_PIN_7, GPIO_PIN_RESET); // turn external oscillator off SysTick->CTRL = 0; while (!(PWR->CSR2 & PWR_CSR2_WUPF4)) // while wakeup pin is not asserted { HAL_GPIO_TogglePin(GPIOE, GPIO_PIN_2); // debug HAL_PWR_EnterSTANDBYMode(); }2017-08-24 3:38 AM
How do you know it's the regulator that pulls the 5mA? In Standby mode the voltage regulator is always disabled and the 1.2V domain is fully powered off.
Also no need to manually switch to HSI from HSE
because when entering into Standby mode HSE, HSI and PLL will be disabled all the same.Edit: Ah, I have never used external oscillator instead of a standard crystal, now I understand why you turn it off before entering into standby.
2017-08-24 5:46 AM
I can see that the regulator stays on by the voltage on the VCAP_1 and VCAP_2 pins.
PA7 enables the external oscillator, which needs to be disabled in standby to reduce power consumption. I cannot turn it off while using it, so I switch to the internal oscillator HSI and then turn it off.
2017-12-07 1:35 AM
bump
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.