cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F765 QSPI Dual Bank with Quad lines Means i have 2 QSPI channels ? I can connect 2 QSPI slaves (1- Flash memory, 2 - FPGA) ?

ER7
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
waclawek.jan
Super User

AFAIK, no.

It is designed so that two QSPI memories can be connected, but they are accessed simultaneously, mimicking 8-bit access.

JW

ER7
Associate II

​Hi JW

Thanks for answering

So as i understood the QSPI interface is for memory only ?

Or i can connect one slave device (like FPGA) instead of memory ?

My understanding is that it can be used in an interleaving mode, but also has two distinct bank pins allowing for different memory types. If the manuals are not clear on this, discuss with an FAE.

I'd expect an FPGA could be used in the same way as a QSPI RAM device.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.