2021-06-17 12:47 AM
I am trying to boot from the QSPI on F7508-DK board.
I followed the guide by ST mentioned at STM32Cube\Repository\STM32Cube_FW_F7_V1.16.1\Projects\STM32F7508-DISCO\Templates\ExtMem_Boot
Basically this needs to be flashed once, so the code can jump from 0x08000000 to 0x90000000.
It is working alright for the examples provided by ST, but when I write my own code, the system clock fails to initialize.
If I comment out the system clock config, even memcopy function is working well.
But again, without the system clock, Other things aren't working.
Solved! Go to Solution.
2021-06-22 10:46 AM
@Imen DAHMEN Thanks for the reply, but I got it working. I forgot to relocate the vector table.
If anyone face this issue, you need to relocate the Vector table in the SystemInit function
SCB->VTOR = QSPI_BASE;
2021-06-22 7:29 AM
Hello @arun singh,
Please provide more details to help you solve your issue.
You can share your source code with clock configuration to check more this behavior.
We would mind having a look at the configuration
Thanks
Imen
2021-06-22 10:46 AM
@Imen DAHMEN Thanks for the reply, but I got it working. I forgot to relocate the vector table.
If anyone face this issue, you need to relocate the Vector table in the SystemInit function
SCB->VTOR = QSPI_BASE;
2021-06-23 1:53 PM
Thanks @arun singh for your update and sharing your solution.
I select your answer as Best. This will help other users find that answer faster.
Thanks
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.