2015-11-12 4:47 AM
I have a problem with the datasize of the SPI of the stm32f746.
When I set the size (DS in CR2) 0111: 8-bit or lower, the spi gives double clock pulses. When I set the size 1000: 9-bit or bigger, the clock pulses are equivalent with the setting of the data size. What should be the problem? The settings are (controlled by reading the regs) : CR1: 0x0074 CR2: 0x1704 I2SCFGR : 0x0000 uint8_t spi_8send(SPI_TypeDef* SPIx, uint8_t data) { SPIx->DR = data; // write data to be transmitted to the SPI data register while(1); blocked, for debugging with the scope, then I see 16 clock pulses while( !(SPIx->SR & SPI_I2S_FLAG_TXE) || (SPIx->SR &SPI_FIFO_FTLVL)); // wait until transmit complete while( !(SPIx->SR & SPI_I2S_FLAG_RXNE) ); // wait until receive complete while( SPIx->SR & SPI_I2S_FLAG_BSY ); // wait until SPI is not busy anymore return SPIx->DR; // return received data from SPI data register }2015-11-12 5:03 AM
According RM0385 chapter 32.5.8 Data transmission and reception, when the size is 8-bit or less, two characters are packed into the 16-bit DR. Using SPIx->DR writes the whole 16-bit, resulting in (almost) the same effect as two 8-bit accesses.
2015-11-26 2:26 AM
Thanks!
It's solved: uint8_t spi_8send(SPI_TypeDef* SPIx, uint8_t data) { *((volatile uint8_t*)&SPIx->DR) = data; // write data to be transmitted to the SPI data register while( !(SPIx->SR & SPI_I2S_FLAG_TXE) || (SPIx->SR & SPI_FIFO_FTLVL)) _spi_printstatus(SPIx); // wait until transmit complete while( !(SPIx->SR & SPI_I2S_FLAG_RXNE) ) _spi_printstatus(SPIx); // wait until receive complete while( SPIx->SR & SPI_I2S_FLAG_BSY ) _spi_printstatus(SPIx); // wait until SPI is not busy anymore return SPIx->DR; // return received data from SPI data register }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.