2016-07-04 12:21 AM
Test Environment
STM32F746G-DiscoveryMDK-ARM, uvision V5.14.0.0 (Licenced)USB High-Speed, Mass Storage Class Example ( ST_STM32F\STM32Cube7\STM32Cube_FW_F7_V1.4.0\Projects\STM32746G-Discovery\Applications\USB_Device\MSC_Standalone\MDK-ARM )1. Compilation works okay with MDK-ARM. 2. Board is powered by 5V_LINK (CN14) and USB-HS is connected via CN12.2. Pressing 'Download' button works okay. 2-1. PC recognizes 'removable disc'3. Test I. 3-1. dis-connect USB-HS (CN12) : 'removable disc' disappears 3-2. and re-connect : PC recognizes it as 'removable disc' 3-3. pressing reset button : during pressing, 'removable disc' disappears 3-4. Releasing reset button : PC recognizes it as 'removable disc'4. Test II. 4-1. Disconnect power (CN14) 4-2. Re-connect power : 'removable disc' is not recognized any more. 4-3. Reset button : no change. 5. I change the compile option to USE_USB_FS 5-1. Item 3 (Test I) and Item 4 (Test II) works okay. From the tests, I suspect - USB HS MSC example code has initialization error, so it doesn't work with power-up. Can you test the Cube_FW_F7_V1.4.0 USB HS MSC example on your STM32F746G discovery and share the result ?Thanks, Best Regards, Danny2016-07-04 6:32 PM
FAE from Korean agent Insem helped me on this topic.
It was caused by ''external power''To use OTG function, I should use external power.I thought - I only use device mode - Right after downloading the firmware, things were okaySo I 'guess' that external power is not necessary. But, I was wrong. After switching to external power, the firmware works okay. Even I power-off and on the board, the firmware works fine.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.