2018-10-06 5:18 AM
Hi,
I am starting to program STM32 devices and I have an STM32F745 chip. Since I want to learn all the details I'm programming it from scratch, using only the definitions from CMSIS.
I have a very simple program where I have 2 LEDs on PB6 and PB7 respectively. Right now I only want to turn them on. I have achieved this compiling the code with "-O0" optimization flag, but when I change it to "-O2" then it doesn't work, the LEDs are off. Here's the code:
#include <stm32f745xx.h>
int main()
{
// Blue LED is on PB7, Red LED is on PB6
// 1) Enable clock for Port B, since input/output are latched
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOBEN;
// 2) Configure PB6 and PB7 as output. Push-pull is default conf on reset
// PortB has value 0x0000 0280 on reset
GPIOB->MODER = 0x0000'5280;
// 3) Wait indefinitely
while(1){}
}Compiling with "-O0" optimization flag, the chip behaves as expected and both LEDs are turned on. I get the following assembly:
08000208 <main>:
8000208: b480 push {r7}
800020a: af00 add r7, sp, #0
800020c: 4b05 ldr r3, [pc, #20] ; (8000224 <main+0x1c>)
800020e: 6b1b ldr r3, [r3, #48] ; 0x30
8000210: 4a04 ldr r2, [pc, #16] ; (8000224 <main+0x1c>)
8000212: f043 0302 orr.w r3, r3, #2
8000216: 6313 str r3, [r2, #48] ; 0x30
8000218: 4b03 ldr r3, [pc, #12] ; (8000228 <main+0x20>)
800021a: f44f 42a5 mov.w r2, #21120 ; 0x5280
800021e: 601a str r2, [r3, #0]
8000220: e7fe b.n 8000220 <main+0x18>
8000222: bf00 nop
8000224: 40023800 .word 0x40023800
8000228: 40020400 .word 0x40020400 When I compile with "-O2", the LEDs are off. I get the following assembly:
08000208 <main>:
8000208: 4a04 ldr r2, [pc, #16] ; (800021c <main+0x14>)
800020a: f44f 40a5 mov.w r0, #21120 ; 0x5280
800020e: 4904 ldr r1, [pc, #16] ; (8000220 <main+0x18>)
8000210: 6b13 ldr r3, [r2, #48] ; 0x30
8000212: f043 0302 orr.w r3, r3, #2
8000216: 6313 str r3, [r2, #48] ; 0x30
8000218: 6008 str r0, [r1, #0]
800021a: e7fe b.n 800021a <main+0x12>
800021c: 40023800 .word 0x40023800
8000220: 40020400 .word 0x40020400In both cases I can see that it's storing the correct values in the registries so I don't understand why the LEDs are not being turned on!
Am I missing something obvious?
Thanks!!
2018-10-06 5:29 AM
There is a documented hazard for writing to a peripheral registers immediately after enabling the clock
2018-10-06 12:05 PM
"both LEDs are turned on."
a pin can be set/cleared for other reasons. it is much more reliable to test code execution by flipping them constantly.
2018-10-06 4:10 PM
> There is a documented hazard for writing to a peripheral registers immediately after enabling the clock
RM0385, 5.2.12 Peripheral clock enable register (RCC_AHBxENR, RCC_APBxENRy):
> Caution: Just after enabling the clock for a peripheral, software must wait for a 2 peripheral clock
> cycles delay before accessing the peripheral registers.
2018-10-07 1:53 AM
That did the trick, thanks a lot!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.