2017-11-27 2:55 AM
Hi all,
I am working with STM32F733x MCU and having trouble achieving the following configuration through HAL library.
Following is what I would like to acheive
1) Synchronise TIM1 (master) & TIM8(slave) in slave trigger mode (TIM_SLAVEMODE_TRIGGER)
2) Use the slave timer TIM8 to trigger ADC1 & ADC2 in dual interleaved & return the ADC samples (12bit) through dma callback
Attached the main.c file generated with the help from stmcube.
I am unable to get the ADC callback triggered
Any pointers?
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.