2016-12-22 12:14 AM
Hi, i'm using Stm32f746zg nucleo-144 board and i want to work with sd card communication, as i see on internet there are some examples about f4 but i did not work with sd card. ?f anybody tried something about sd card in F7 or would you like to share projects about sdmmc1. I did same in this video(
) but not works. Thanks a lot #stm32f746-nucleo2016-12-22 5:07 AM
I'm sure, you can use most of the Drivers for STM32L4/F4 or other Controllers with SDMMC also for your STM32F7. Only the real LowLevel-Drivers could be different and they come from Cube and I would suggest you to not change them. The above Layers must be fixed to your Needs. The only half-working Example from STM are the one Part of the CubeL4-FW for the big and expansive STM32-L476-Eval-Board. All other Examples for F4/L4 as far as I know (and I tested a lot) do not work. The generated Code is also not working. So use the one from the big L476-Eval-Board. Most important for you is the diskio-Layer.
You can also take a look into some Informations around SDMMC for L4 in this Thread:
https://community.st.com/0D70X000006SzQWSA0
You should arrange some time for getting it to work stable and fast ...
2016-12-22 5:16 AM
That was helpful. Thanks a lot.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.