2015-08-17 2:08 AM
I have a STM32F746G DISCOVERY board and am starting to use System Workbench. I have found that in the STM32Cube_FW_F7_V1.1.0 folder for the DSP library CMSIS/GCC there is only the M4 library, but in the CMSIS/ARM folder there are newer M7 libraries.
Where are the GCC libraries for the M7 ?Charles Putney2015-08-17 5:38 AM
The F7 uses a single-precision FPU, so I don't see it having materially more functionality than an M4.
Source is provided, right?2015-08-17 12:26 PM
Yes, there is source in the DSP-Lib folder but for the fft transform files the header says ''Target Processor: Cortex-M4/Cortex-M3/Cortex-M0''. In the ''Lib'' folder which has the compiled libraries for ARM and GCC, in the ARM folder there are 6 compiled libraries:
arm_cortexM7b_math.libarm_cortexM7bfdp_math.libarm_cortexM7bfsp_math.libarm_cortexM7l_math.libarm_cortexM7lfdp_math.libarm_cortexM7lfsp_math.libI don't think the source matches the libraries. Also, in numerous press releases, it said that ''STM32 F7 Cube, a new CMSIS DSP library, discovery kits ...'', so where is the new library ?I have looked on the ARM site and the only CMSIS I see is ''CMSIS-SP-00300-r4p3-00rel0'' and it doesn't have the GCC libraries or the correct source either.2015-08-17 1:05 PM
The only library of any merit for the F7 is the arm_cortexM7lfsp_math.lib
__TARGET_CPU_CORTEX_M7_FP_SP 1__TARGET_FPU_FPV4_SP 1ARMCM7_SP 1ARM_MATH_CM7 1ARM_MATH_MATRIX_CHECK 1ARM_MATH_ROUNDING 1__FPU_PRESENT 1Five of the source files have a dependency on ARM_MATH_CM7 in their build/structurearm_biquad_cascade_df2T_f32.carm_biquad_cascade_df2T_f64.carm_biquad_cascade_stereo_df2T_f32.carm_cfft_radix4_q31.carm_fir_f32.cThe GNU/GCC build is missing, but I think it possible to synthesize from the supplied source.Salient command line parameters to translate:--cpu=Cortex-M7.fp.sp --fpu=FPv4-SP --fpmode=ieee_full-DARMCM7_SP -DARM_MATH_CM7 -DARM_MATH_MATRIX_CHECK -DARM_MATH_ROUNDING -D__FPU_PRESENT=12015-08-17 2:27 PM
Attached is libarm_cortexM7lfsp_math.a
Built this with the V1.4.4 CMSIS DSP Library, and GNU C 4.9.3 ________________ Attachments : libarm_cortexM7lfsp_math.a : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0g0&d=%2Fa%2F0X0000000bcf%2F.dTlCVW_ZrqdgTznJ43ppjSdUoVhVWkU8pHfkZ9GWd8&asPdf=false2015-08-18 2:23 AM
Thank you for this help.
2015-08-18 10:30 AM
I have looked on the ARM site and the only CMSIS I see is ''CMSIS-SP-00300-r4p3-00rel0'' and it doesn't have the GCC libraries or the correct source either.
This contains the DSP V1.4.5 version, GNU/GCC users are expected to build their own, and ARM's comments on the CMSIS page tell me they are only going to test/validate the ARM (Keil) built libraries. The source is buildable, but doesn't come with instructions for your average user. Attached is a library build using the setting/options from V1.4.5 /* From Keil (GNU/GCC) CMSIS DSP V1.4.5 project -fno-strict-aliasing -ffunction-sections -fdata-sections -mfpu=fpv5-sp-d16 -mfloat-abi=hard -ffp-contract=off ARM_MATH_CM7, ARM_MATH_MATRIX_CHECK, ARM_MATH_ROUNDING, UNALIGNED_SUPPORT_DISABLE, __FPU_PRESENT = 1 */ ________________ Attachments : libarm_cortexM7lfsp_math.a : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0hb&d=%2Fa%2F0X0000000bce%2F6rgVf4RgmHNwveIOoB7XXAKVF.TZ1Bm7aDYn_.OPWhQ&asPdf=false
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.