2016-07-08 9:04 AM
I'm developing an audio application using STM32F427, using I2S port 3 in ''full-duplex'' mode to interface to ADC and DAC.
Trying to use the non-blocking-interrupt method, as I don't want to use DMA and there are several related functions in the same RTOS thread that I don't want to block. On trying to trace the interrupt handling code, as far as I can see, the function I2SEx_TransmitReceive_IT doesn't contain any callback calls in the I2S_MODE_MASTER_TX or I2S_MODE_SLAVE_TX section. There are callbacks in the RX section, but they leave the peripheral in HAL_I2S_STATE_BUSY - which will cause any call to HAL_I2SEx_TransmitReceive_IT (in order to re-start transmission/reception) to fail. It also leaves the macro __HAL_LOCK(hi2s) in the locked state. I have searched through this forum history and can't see any solution. I did see a related question, but the poster got round it by using DMA. I'm using code originally created by CUBE FW.F4_V1.11.0, which uses HAL version 1.4.4. I downloaded the latest CUBE (version 1.12), with HAL version 1.5.0 - but the included code is identical. Any chance of some fully complete and working HAL files? Or have I missed something?2016-07-15 8:08 AM
Hi fleetwood.mike,
Thanks for highlighting this issue. It is reported internally to be fixed in one of coming releases of the STM32CubeF4 package.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2016-07-17 10:57 PM
Same issue with an STM32F051 app.
We used HAL_I2C_Master_Transmit / HAL_I2C_Master_Receive in the end to read 20bytes from a AS5600 magnetic encoder chip. This works fine in the beginning. After several readings an extra 0x00 byte is in the reception buffer at start which is not visible using a scope. We have no time to investigate this at this moment, so we use a patch to ignore this byte since the result of the chip is never 0x00 at start..2016-07-18 2:44 AM
Hi Werner Meier,
This is an I2S related issue/topic (not I2C).Could you please start a new thread in which you describe exactly the problem you are facing? If it is already done, please provide the link.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2016-07-18 6:22 AM
Ups sorry..
for I2C in interrupt mode, it worked one time, then stayed also got stuck in HAL_I2C_STATE_BUSY mode.. I will open a new topic2016-08-01 5:10 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.