2014-05-19 5:04 AM
Hello Everyone,
I was just wondering if anyone has seen this, I have seen this only referenced on one website. I have SPI1 on a STM32F415 configured as PA7 ------> SPI1_MOSI PB3 ------> SPI1_SCK PB4 ------> SPI1_MISO Which works fine until i configure PE3, as soon as I do that the SPI1 stops working if I comment the following out it will work again. /*Configure GPIO pins : PE3 */// GPIO_InitStruct.Pin = GPIO_PIN_3;// GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;// GPIO_InitStruct.Pull = GPIO_NOPULL;// GPIO_InitStruct.Speed = GPIO_SPEED_FAST;// HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);I haven't seen no errata about it, am I the only one seeing this?Thanks,George2014-05-19 5:24 AM
Post a minimal, but complete compilable example which exhibits the problem.
You might also want to post the link to the mentioned website. JW2014-05-19 6:11 AM
Hi the following is a link to the minimal project, to exhibit the behavior un-comment the PE3 Configuration code in main::MX_GPIO_Init()
https://drive.google.com/file/d/0B9AbQf-Nlf0KQ0ZJOWFaVjlfUlE/edit?usp=sharing
Thank You,George2014-05-19 6:50 AM
Code looks reasonable.
What exactly are the symptoms of ''not working''? Did you check the signals with an oscilloscope? Can't there be a hardware issue, e.g. PE3 shorted onto some of the SPI lines? JW2014-05-19 7:02 AM
I haven't seen no errata about it, am I the only one seeing this?
Assume you are, and provide details about the board or anything else unique to your situation that you would need to communicate to a third-party for them to be able to independently analyzer and verify the issue. Most Cube/HAL related support is occurring on the other STM32 Forum page.2014-05-19 7:27 AM
What is connected to PE3?
Don't you use a DISCOVERY board, by chance? There is an error in the table indicating the pins' connections, related to PE3. JW2014-05-19 7:28 AM
Related thread, but abandoned without resolution: https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FSTM32F4%20Bug%20with%20SPI1&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=205
2014-05-19 7:47 AM
Related thread, but abandoned without resolution
Jan thanks for the link. Indicates we're not alone, but still really not enough meat to suggest it's a chip errata and not a circuit board level issue.2014-05-19 8:59 AM
2014-05-19 9:11 AM
I have an Accelerometer CS line hooked to PE3, the issue is if I am not using the pin for anything and when I initialize the pin in the test program i set it as output with nopull (which should leave it floating). I did verify that there is no shorts, I will need to hook up the scope again and see what it looks like in both states.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.