2016-09-14 12:57 PM
Hi
I am attempting to develop application on STM32F469II that utilizes USB CDC.On our HW board, i am able to run STM CubeMX CDC Standalone example.But we are using Keil toolchain, and when running Keil based example - i am not even geting USB RESET (USBRST
). I have exactly the same clock configuration (copied SystemClockUpdate) function from Cube to Keil...What can be a reason for such a behavior where even USBRST is not happening?We are using FS mode of USB and CDC Device configurationKeil driver for USB is 6.8.0Appreciate any help...Igor2016-09-16 1:07 AM
Hi igor.igor.002,
Is there any warning or error message ? (the USB wouldn't enumerate then ?) Have you checked the USBRST bit in the OTG_FS_GINTSTS register ? As a test for your hardware, try to run a ready to use example in the STM32Cube and see if it works . -Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.