2021-06-23 3:52 AM
Hello everyone,
I'm currently developing a project using Touchgfx on a custom board with a STM32F469II, external RAM/FLASH, SD card and a 1024x600 screen.
I'm having trouble placing the frame buffer in the external RAM close to eachover. Right now, the following configuration in the "TouchGFXHAL.cpp" is working quite well:
setFrameBufferStartAddresses((void*)0xC0000000, (void*)0xC0200000, (void*)0xC0400000);
The parameters are as follow:
- The first address is the start of the first frame buffer.
- The second address is the start of the second frame buffer (use for multi-buffering).
- The third address is the start of the animation storage space (use for slide transition between screen).
All of them are placed in the external RAM space of the custom board which goes from 0xC0000000 to 0xC07FFFFF (8 MB).
With that, a fourth and final space is added which is the dynamic bitmap cache which stores images from the SD card to be displayed over the screen with TouchGFX.
Howerver, when I want to maximize that fourth space to get as much place as possible to store images from the SD card (as an example, backgrounds which take a lot of space), I'm having a lot of trouble decreasing the space between the framebuffers, here's what I've found out so far:
I'v already contacted the screen manufacturer which told me that it could be dut to the fact that DMA2D can be configured to 8/16/32 -bit access and a wrong alignement could explain the jitters. However, since he's not quite sure how to check the DMA2D access size and if it's really what's causing the shaking, I'm asking here if anyone ever experienced that issue and if so how to fix this problem.
Thanks in advance,
DELETRAZ Tristan
Solved! Go to Solution.
2021-06-23 7:50 AM
You need read LTDC appnotes , and FYI LTDC need that framebuffer start address meet some conditions. For example cant **** by one byte or word...
Second condition is FMC SDRAM access on banks and optimal is every buffer on separated bank. On your SDRAM maybe one bank is 2M and have four.
When you need you can only go down with framerate aka dotclock and then LTDC and FMC can cooperate with other address , but this need meet basic condition, for example must be multiply of 64...
2021-06-23 7:50 AM
You need read LTDC appnotes , and FYI LTDC need that framebuffer start address meet some conditions. For example cant **** by one byte or word...
Second condition is FMC SDRAM access on banks and optimal is every buffer on separated bank. On your SDRAM maybe one bank is 2M and have four.
When you need you can only go down with framerate aka dotclock and then LTDC and FMC can cooperate with other address , but this need meet basic condition, for example must be multiply of 64...
2021-06-23 8:15 AM
Thanks a lot for the anwser. I didn't know about the condition where the frame buffers should be in different banks.
Tristan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.