2017-02-03 10:44 AM
I have my clock setup for 168MHz and I see that with a scope at MD0. But a call to BSP_CPU_ClkFreq() indicates it is running at 550 MHz. This is the setup I have in bsp.c:
// Configure for 8MHz XTAL => 168MHz SysClk
#define BSP_BIT_RCC_PLLCFGR_PLLM 4u#define BSP_BIT_RCC_PLLCFGR_PLLN 168u#define BSP_BIT_RCC_PLLCFGR_PLLP 2u#define BSP_BIT_RCC_PLLCFGR_PLLQ 7u RCC_DeInit(); RCC_HSEConfig(RCC_HSE_ON); /* HSE = 8MHz ext. crystal. */ RCC_WaitForHSEStartUp();RCC_HCLKConfig(RCC_SYSCLK_Div1); /* HCLK = AHBCLK = PLL / AHBPRES(1) = 168MHz. */
RCC_PCLK2Config(RCC_HCLK_Div2); /* APB2CLK = AHBCLK / APB2DIV(2) = 84MHz. */ RCC_PCLK1Config(RCC_HCLK_Div4); /* APB1CLK = AHBCLK / APB1DIV(4) = 42MHz (max). *//* PLLCLK = HSE * (PLLN / PLLM) = 336MHz. */
/* SYSCLK = PLLCLK / PLLP = 168MHz. */ /* OTG_FSCLK = PLLCLK / PLLQ = 48MHz. */ RCC_PLLConfig(RCC_PLLCFGR_PLLSRC_HSE, BSP_BIT_RCC_PLLCFGR_PLLM, BSP_BIT_RCC_PLLCFGR_PLLN, BSP_BIT_RCC_PLLCFGR_PLLP, BSP_BIT_RCC_PLLCFGR_PLLQ);RCC_PLLCmd(ENABLE);
while (RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET) { /* Wait for PLL to lock. */
; }FLASH_SetLatency(FLASH_Latency_5); /* 5 Flash wait states when HCLK > 120MHz. */
FLASH_PrefetchBufferCmd(ENABLE);RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK); /* HCLK = SYSCLK = PLL = 168MHz. */
while (RCC_GetSYSCLKSource() != RCC_CFGR_SWS_PLL) { ; }Solved! Go to Solution.
2017-02-03 10:48 AM
Ensure the HSE_VALUE define is 8000000, not 25000000
2017-02-03 10:48 AM
Ensure the HSE_VALUE define is 8000000, not 25000000
2017-02-03 3:31 PM
The header file stm32f4xx.h insists that 25000000 is the right number for the stm32f437. But not anymore....
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.