2018-06-08 7:37 AM
Hi, guys.
I am using STM32F437 and trying to use PI8 as an output port.
I am trying to program it using standard procedures:
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOI, ENABLE);
GPIO_InitTypeDef GPIO_InitStructure; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_Init(GPIOI, &GPIO_InitStructure); GPIOI->BSRRL=GPIO_Pin_8; // Set logical 1As the result, I see always logical 0 on the output.
I know that this pin has some additional features from RTC.
What should I do to use this port as standard IO in output mode?
Regards, George.
#stm32f437-and-pi82018-06-08 9:10 AM
It is in the low power domain is has low current drive capabilities.
What are you driving it into?
Use an external buffer.
In a no load condition, toggle it and scope
while(1) GPIOI->ODR ^=GPIO_Pin_8;
2018-06-08 11:58 AM
I have only an external 10k pullup resistor on this pin, its output is always logical 0.
What is wrong? Should I do anything additional to switch this pin to IO mode?
2018-06-08 12:38 PM
I don't believe there is anything special that needs to be done, it is not a part I have access to.
The PI8 pin is not bonded out in several packages, your part number is insufficiently complete for me to make a specific determination.
2018-06-08 4:30 PM
on my new board PI8 is Tamper2, so it is a little special.
I didnt run it up yet, I hope it works...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.