2020-01-28 9:52 AM
MCU sets FLASH->SR bits: PGPERR and PGSERR all the time even immediately after it is cleared.
It causes a problem with erasing flash memory.
I am using RTOS(TIM1 as a base), Timers and Systick as well but I think those shouldn't be a problem.
Code is executed from flash but from different regions, so it isn't overlapping.
I was thinking if cache can make this problem, but after turning of cache before I have still the problem.
I was doing flashing other sectors on STM32F1 and there was no problems with it, but if I remember correctly there are no such flags.
2020-01-28 11:38 AM
I suspect there is a corrupted or uninitialized pointer somewhere that tries to write the flash.
If it's a null pointer, you can catch it by mapping RAM at address 0, see SYSCFG->MEMRMP. Move the beginning of the RAM up by a few words in the linker script, place some guard value at 0x20000000, and see if it changes.
2020-01-28 1:28 PM
The clue seems to be good. I had no time to do exactly what you mentioned yet, but I turned off some tasks and I think the guilty one is default task with LWIP initialization (because it looks that it helped). I would need to investigate more because I would need to have both Ethernet and Flashing at same time.
2020-05-29 4:16 AM
Thanks for sharing this answer. This thread and the following thread solved a similar issue of me:
It was actually a bug introduced by me:
I have a watchdog running and reset it frequently with
HAL_IWDG_Refresh(&hiwdg);For debugging purpose, I disable my watchdog init
// disable for debugging purpose
// MX_IWDG_Init();This causes problem in the Flash interface, where the FLASH_WaitForLastOperation() function fails.
My solution is to also disable the HAL_IWDG_Refresh() function in debugging.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.