2014-11-07 8:37 PM
I waited for a 208 pin version for about a year and it is still not available (RUTRONIC now has 14 weeks wait time). So I want to try the STM32F429I (176 pins) for driving an RGB888 LCD with 32-bit SDRAM. It is ''kinda'' possible if I sacrifice byte select in the FMC controller. According to the manual I can live without it because a) read mode does not use it and b) for writing I can always align my data to a 4-byte boundary. The question is, will the SDRAM controller work with byte select disabled/uninitialized?
2014-11-07 8:54 PM
They all share the same die, so you could route to pins that don't exist, or simply mux a different AF to a given pin. I don't think the controller cares if outputs escape the part, or not.
2014-11-08 11:36 AM
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.