2015-12-17 5:03 AM
Hi Guys.
I recently picked up the above-mentioned evaluation board. I am currently using TrueStudio. I want to display text strings on the on-board LCD. I have been trying to butcher one of the examples to include and use ''stm32f429i_discovery_lcd.h'' library but without any success. I seem to run into all kinds of issues when trying to compile. Does anyone have an example regarding which files should be included and in which sequence do I initialize to display text on the screen? This is what I currently have, but not yet compiling. I will update as soon as I have something that compiles. Help would be greatly appreciated.. Thanks! AJBotha
/**
******************************************************************************
* @file EXTI_Example/main.c
* @author MCD Application Team
* @version V1.0.0
* @date 20-September-2013
* @brief This example shows how to configure external interrupt lines.
******************************************************************************
* @attention
*
* <h2><center>© COPYRIGHT 2013 STMicroelectronics</center></h2>
*
* Licensed under MCD-ST Liberty SW License Agreement V2, (the ''License'');
* You may not use this file except in compliance with the License.
* You may obtain a copy of the License at:
*
* http://www.st.com/software_license_agreement_liberty_v2
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an ''AS IS'' BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*
******************************************************************************
*/
/* Includes ------------------------------------------------------------------*/
#include ''main.h''
#include ''stm32f429i_discovery_lcd.h''
#include ''fonts.h''
/** @addtogroup STM32F429I_DISCOVERY_Examples
* @{
*/
/** @addtogroup EXTI_Example
* @{
*/
/* Private typedef -----------------------------------------------------------*/
EXTI_InitTypeDef EXTI_InitStructure;
/* Private define ------------------------------------------------------------*/
/* Private macro -------------------------------------------------------------*/
__IO uint32_t TimingDelay;
/* Private variables ---------------------------------------------------------*/
/* Private function prototypes -----------------------------------------------*/
static
void
EXTILine0_Config(
void
);
static
void
EXTILine13_Config(
void
);
/* Private functions ---------------------------------------------------------*/
/**
* @brief Main program
* @param None
* @retval None
*/
int
main(
void
)
{
/*!< At this stage the microcontroller clock setting is already configured,
this is done through SystemInit() function which is called from startup
files (startup_stm32f429_439xx.s) before to branch to application main.
To reconfigure the default setting of SystemInit() function, refer to
system_stm32f4xx.c file
*/
RCC_ClocksTypeDef RCC_Clocks;
/* SysTick end of count event each 1ms */
RCC_GetClocksFreq(&RCC_Clocks);
SysTick_Config(RCC_Clocks.HCLK_Frequency / 1000);
BSP_LCD_Init();
BSP_LCD_LayerDefaultInit(0, (uint32_t) LCD_FRAME_BUFFER);
BSP_LCD_SelectLayer(0);
BSP_LCD_SetLayerVisible(0,ENABLE);
BSP_LCD_DisplayOn();
BSP_LCD_Clear(LCD_COLOR_RED);
BSP_LCD_DisplayChar(1,1,0x41);
BSP_LCD_DisplayStringAt(2,2, (uint8_t *)
''Hello!''
, CENTER_MODE);
LCD_SetLayer(0);
LCD_DisplayOn();
LCD_SetTextColor(5-6-5);
LCD_DisplayStringLine(2, (uint8_t *)
''Test Display''
);
/* Initialize LEDs mounted on EVAL board */
STM_EVAL_LEDInit(LED3);
STM_EVAL_LEDInit(LED4);
/* Put LED3 on */
STM_EVAL_LEDOn(LED3);
/* Configure EXTI Line0 (connected to PA0 pin) in interrupt mode */
EXTILine0_Config();
/* Configure EXTI Line13 (connected to PC13 pin) in interrupt mode */
EXTILine13_Config();
while
(1)
{
/* Generate software interrupt: simulate a falling edge applied on EXTI0 line */
EXTI_GenerateSWInterrupt(EXTI_Line13);
Delay(500);
}
}
/**
* @brief Configures EXTI Line0 (connected to PA0 pin) in interrupt mode
* @param None
* @retval None
*/
static
void
EXTILine0_Config(
void
)
{
EXTI_InitTypeDef EXTI_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
/* Enable GPIOA clock */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
/* Enable SYSCFG clock */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);
/* Configure PA0 pin as input floating */
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Connect EXTI Line0 to PA0 pin */
SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOA, EXTI_PinSource0);
/* Configure EXTI Line0 */
EXTI_InitStructure.EXTI_Line = EXTI_Line0;
EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;
EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising;
EXTI_InitStructure.EXTI_LineCmd = ENABLE;
EXTI_Init(&EXTI_InitStructure);
/* Enable and set EXTI Line0 Interrupt to the lowest priority */
NVIC_InitStructure.NVIC_IRQChannel = EXTI0_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x0F;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x0F;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
}
/**
* @brief Configures EXTI Line15 (connected to PG15 pin) in interrupt mode
* @param None
* @retval None
*/
static
void
EXTILine13_Config(
void
)
{
EXTI_InitTypeDef EXTI_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
/* Enable GPIOC clock */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
/* Enable SYSCFG clock */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);
/* Configure PC13 pin as input floating */
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13;
GPIO_Init(GPIOC, &GPIO_InitStructure);
/* Connect EXTI Line15 to PC13 pin */
SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOC, EXTI_PinSource13);
/* Configure EXTI Line13 */
EXTI_InitStructure.EXTI_Line = EXTI_Line13;
EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;
EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Falling;
EXTI_InitStructure.EXTI_LineCmd = ENABLE;
EXTI_Init(&EXTI_InitStructure);
/* Enable and set EXTI15_10 Interrupt to the lowest priority */
NVIC_InitStructure.NVIC_IRQChannel = EXTI15_10_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x0F;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x0F;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
}
/**
* @brief Inserts a delay time.
* @param nTime: specifies the delay time length, in 10 ms.
* @retval None
*/
void
Delay(__IO uint32_t nTime)
{
TimingDelay = nTime;
while
(TimingDelay != 0);
}
/**
* @brief Decrements the TimingDelay variable.
* @param None
* @retval None
*/
void
TimingDelay_Decrement(
void
)
{
if
(TimingDelay != 0x00)
{
TimingDelay--;
}
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void
assert_failed(uint8_t* file, uint32_t line)
{
/* User can add his own implementation to report the file name and line number,
ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */
/* Infinite loop */
while
(1)
{
}
}
#endif
/**
* @}
*/
/**
* @}
*/
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
#discovery #!stm32-!lcd-!tft-!discovery-! #stm32f429i #stm32
2015-12-17 5:57 AM
These are the compile errors that I get. I checked the location of the ili9h and the file is there, don't know why the compiler can't find it? I think the sdram error is the real issue. 15:34:11 **** Incremental Build of configuration Debug
for project STM32F429I-Discovery ****Info: Internal Builder
is used for build arm-atollic-eabi-gcc -c -mthumb -mcpu=cortex-m4 -mfloat-abi=softfp -mfpu=fpv4-sp-d16 -std=gnu90 -DUSE_HAL_DRIVER -DSTM32F429xx -DUSE_STM32F429I_DISCO -I..\..\..\Inc -I..\..\..\..\..\..\..\..\Drivers\CMSIS\Device\ST\STM32F4xx\Include -I..\..\..\..\..\..\..\..\Drivers\STM32F4xx_HAL_Driver\Inc -I..\..\..\..\..\..\..\..\Drivers\BSP\STM32F429I-Discovery -I..\..\..\..\..\..\..\..\Drivers\CMSIS\Include -Os -ffunction-sections -fdata-sections -g -Wall -Wno-unused-but- set -variable -Wno-unused-variable -o Example\User\main.o ..\..\..\Src\main.c In file included from ..\..\..\..\..\..\..\..\Drivers\BSP\STM32F429I-Discovery/stm32f429i_discovery_lcd.h:50:0, from ..\..\..\Src\main.c:41: ..\..\..\..\..\..\..\..\Drivers\BSP\STM32F429I-Discovery/stm32f429i_discovery_sdram.h:153:37: error: unknown type name 'FMC_SDRAM_CommandTypeDef' HAL_StatusTypeDef BSP_SDRAM_Sendcmd(FMC_SDRAM_CommandTypeDef *SdramCmd); ^ In file included from ..\..\..\Src\main.c:41:0: ..\..\..\..\..\..\..\..\Drivers\BSP\STM32F429I-Discovery/stm32f429i_discovery_lcd.h:53:46: fatal error: ../Components/ili9341/ili9h: No such file or directory #include ''../Components/ili9341/ili9h'' ^ compilation terminated.15:34:11 Build Finished (took 258ms)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.