2014-10-21 12:55 AM
I have a board based on the stm32f429. There is a 16M Bytes SDRAM (MT48LC16M8) and a 32M bytes NAND (NAND128W3A2B) connected to the FMC bus.
I used one area of the SDRAM as the LTCD buffer,such as: /* Start Address configuration : the LCD Frame buffer is defined on SDRAM */ LTDC_Layer_InitStruct.LTDC_CFBStartAdress = LCD_FRAME_BUFFER; There is two strange problem: [1] The nand write/read is always unstable, sometimes went wrong. After months of trying, I finally found that: The nand operation is ok if I turn off the LTDC controller, namely not using the SDRAM as frame buffer. the command is: LTDC_Cmd(ENABLE); [2] Even I turn off the LTDC controller, if I use the upper 8M bytes of sdram, the nand still generates write error. To summarize: The only working nand operation is to satisfy both: a. Turn off the LCD controller; b. configure the SDRAM as using 8M bytes only: FMC_SDRAMInitStructure.FMC_ColumnBitsNumber = FMC_ColumnBits_Number_9b; FMC_SDRAMInitStructure.FMC_RowBitsNumber = FMC_RowBits_Number_12b; If I configure to use the whole 16M SDRAM like: FMC_SDRAMInitStructure.FMC_ColumnBitsNumber = FMC_ColumnBits_Number_10b; FMC_SDRAMInitStructure.FMC_RowBitsNumber = FMC_RowBits_Number_12b; nand will go wrong. I have researching this problem for months, can't find the answer, could anyone help me out. Even a hint maybe will help me find the solution. Thank you very much! If I only use the2014-11-18 8:46 AM
So the only solution for me is to wait the version 3 chip?
This is a conversation you should be having with your local ST representatives and FAEs. They are much better placed to understand the problem, and any solutions, or timing of chip releases.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.