2018-03-26 6:10 PM
What is the logic level of GPIO pins of STM32F429 during powering on?
I am using several GPIO pins as enable pins to enable downstream devices. These GPIOs must be 'LOW' during power on until the firmware actively enables them.
I tried to find information from datasheet, but this information is not specified. My question is: when STM32F429 is being powered on and before the firmware takes care of GPIO configurations, what is the status of GPIO, HIGH, LOW or HIGH Z?
Thank you.
2018-03-27 12:46 AM
Unless it's one of the JTAG/SWI pins, and unless you enable bootloader, they are floating - see RM0090 rev.15, 8.3.1 General-purpose I/O (GPIO).
Use an external pulldown if you need a defined logic level during powerup.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.