2019-07-30 11:54 PM
Hello,
I want to convert on ADC1 some channels in regular mode all the time. After a last Transfer request DMA2 Stream 0 should write all converted values in a global buffer. I also want to convert four ADC channels synchronous with injeced mode. So I have ADC_Channel_8 and ADC_Channel_3 in ADC1 and ADC_Channel_9 and ADC_Channel_4 in ADC2. An external trigger, should trigger both ADC synchronous and with the DiscMode I would like convert the channels trigger by trigger.
I found out the I have some error on my converted values. So I see a little part of the converted value from ADC_Channel_4 on ADC_Channel_9 (ADC2 injected conversion). If I uncomment the initialisation from the regular ADC1, so I have on ADC1 and ADC2 only injected conversions then the error is on both ADCs.
/* ADC Common Init */
ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;
ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div4;
ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;
ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;
ADC_CommonInit(&ADC_CommonInitStructure);
/* ADC1 regular configuration */
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ScanConvMode = ENABLE;
ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;
ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfConversion = 0;
ADC_Init(ADC1, &ADC_InitStructure);
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ScanConvMode = ENABLE;
ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;
ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfConversion = 0;
ADC_Init(ADC2, &ADC_InitStructure);
/* ADC1 regular channels 3, 4 configuration */
// ADC_RegularChannelConfig(ADC1, ADC_Channel_5 , 1, ADC_SampleTime_28Cycles);
// ADC_RegularChannelConfig(ADC1, ADC_Channel_14, 2, ADC_SampleTime_28Cycles);
// ADC_RegularChannelConfig(ADC1, ADC_Channel_7 , 3, ADC_SampleTime_28Cycles);
// ADC_RegularChannelConfig(ADC1, ADC_Channel_15, 4, ADC_SampleTime_28Cycles);
// ADC_RegularChannelConfig(ADC1, ADC_Channel_11, 5, ADC_SampleTime_28Cycles);
// ADC_RegularChannelConfig(ADC1, ADC_Channel_6 , 6, ADC_SampleTime_28Cycles);
//
// ADC_DMACmd(ADC1, ENABLE);
// ADC_DMARequestAfterLastTransferCmd(ADC1, ENABLE);
ADC_InjectedSequencerLengthConfig(ADC1, 2);
ADC_InjectedChannelConfig(ADC1, ADC_Channel_8, 1, ADC_SampleTime_15Cycles);
ADC_InjectedChannelConfig(ADC1, ADC_Channel_3, 2, ADC_SampleTime_15Cycles);
ADC_ExternalTrigInjectedConvConfig(ADC1, ADC_ExternalTrigInjecConv_T3_CC4);
ADC_ExternalTrigInjectedConvEdgeConfig(ADC1, ADC_ExternalTrigInjecConvEdge_RisingFalling);
ADC_InjectedDiscModeCmd(ADC1, ENABLE);
ADC_InjectedSequencerLengthConfig(ADC2, 2);
ADC_InjectedChannelConfig(ADC2, ADC_Channel_9, 1, ADC_SampleTime_15Cycles);
ADC_InjectedChannelConfig(ADC2, ADC_Channel_4, 2, ADC_SampleTime_15Cycles);
ADC_ExternalTrigInjectedConvConfig(ADC2, ADC_ExternalTrigInjecConv_T3_CC4);
ADC_ExternalTrigInjectedConvEdgeConfig(ADC2, ADC_ExternalTrigInjecConvEdge_RisingFalling);
ADC_InjectedDiscModeCmd(ADC2, ENABLE);
/* Enable ADC1 */
ADC_Cmd(ADC1, ENABLE);
/* Enable ADC2 */
ADC_Cmd(ADC2, ENABLE);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.