2012-08-10 2:56 AM
Hi,
im using the stm32f41ig-eval board an i modified the example: STM32F4x7_ETH_LwIP_V1.0.0/ FreeRTOS httpserver_socket. After the modification i can send data to the server an it send it back to the client. Than i measured thethroughput
with wireshark and the result is i only got 5Mbit/s throughput. So i modified the file stm32f4x7eth_bsp and un comment the lines: ETH_InitStructure.ETH_Speed = ETH_Speed_100M; ETH_InitStructure.ETH_Mode = ETH_Mode_FullDuplex; but after that i havent yet the 100Mbit/s. So what can i do to get the 100Mbit/s? Oh and my computer I have checked he is configured for 100Mbit/s. please be kind to me i not a native speaker. Thanks IngoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.