2024-01-01 5:08 PM
I'm using the STM32F412 with an SPI LCD on a custom board and am having problems with the SPI communications. It seems that the TXE flag is always high, and therefore the code locks on the -:
while (!__HAL_SPI_GET_FLAG(&spiHal, SPI_FLAG_TXE))
2024-01-01 5:48 PM
> It seems that the TXE flag is always high
High or low? The code you posted will wait until it's high, which is the default state of TXE. No problem there, code won't hang if TXE is high.
Assuming you meant low: Is it initialized and enabled? TXE staying low would indicate it's not active, or misconfigured. Show the contents of the SPI registers at the time of the error.
2024-01-03 2:13 PM
Thanks for the response. You're correct - the check is negative, but the issue is the same as the code locks on the line I mentioned above because the TXE flag is always showing not empty which is the base of the issue.
I'm using a library that worked fine with the 32F410 - of course the problem with using someone elses library is without digging through the code to find what it does, it's impossible to say if it enables everything (or anything!) but I expected it to work similarly to the F410. I added some code to explicitly enable the SPI2 - the code was autogenerated by the Cube IDE so I assume this is correct. This doesn't help and it still locks on the same line with the TXE flag low and BUSY is low (not busy).
I ported some code across to the CubeIDE using the HAL SPI calls, and it works there, so the hardware is fine. My guess is that there's a low level configuration issue - as above - I've taken the autogenerated code from CubeIDE that configures the clocks and SPI and put that into the PlatformIO code, and it seems to run, but the HAL SPI Transmit still times out... I think this points to a low level config issue so I'll keep digging there...
2024-01-03 2:43 PM
All STM32F4 chips have the same SPI peripheral. That's not the issue.
> it's impossible to say if it enables everything
Why? Can't you look at it?
Sounds like the peripheral isn't enabled, or is in slave mode.
2024-01-03 5:48 PM
@TDK wrote:All STM32F4 chips have the same SPI peripheral. That's not the issue.
> it's impossible to say if it enables everything
Why? Can't you look at it?
Sounds like the peripheral isn't enabled, or is in slave mode.
I can look through the source, of course - that was my point above immediately prior to the part you quoted -:
without digging through the code to find what it does, it's impossible to say if it enables everything
If you're suggesting doing something to read back the status, I'd appreciate it if you can state specifically what you suggest I "look at". As I said, I have enabled the SPI using the code generated by the IDE and that works fine when run in the STM IDE, but not when run under PlatformIO.
The code that I'm using to enable this is -:
hspi2.Instance = SPI2;
hspi2.Init.Mode = SPI_MODE_MASTER;
hspi2.Init.Direction = SPI_DIRECTION_2LINES;
hspi2.Init.DataSize = SPI_DATASIZE_8BIT;
hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi2.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi2.Init.NSS = SPI_NSS_SOFT;
hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi2.Init.TIMode = SPI_TIMODE_DISABLE;
hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi2.Init.CRCPolynomial = 10;
if (HAL_SPI_Init(&hspi2) != HAL_OK)
{
Error_Handler();
}
@TDK wrote:Sounds like the peripheral isn't enabled, or is in slave mode.
Again, this code does work when running under the STM IDE - the same code runs fine in PlatformIO, but the SPI doesn't work. If you can advise what I should check, that would be appreciated.
Thanks.
2024-01-03 8:50 PM
> If you're suggesting doing something to read back the status, I'd appreciate it if you can state specifically what you suggest I "look at".
Here's what I suggested in the first post:
> Show the contents of the SPI registers at the time of the error.
What this would do is show the state of the peripheral, including configuration and current status. Since the peripheral runs based solely on the state of the registers, this provides complete information, at least in determining if/how the peripheral is configured.
Showing the HAL initialization code is okay, but clearly there's something else amiss and examining the registers directly will shed light as to what that is. Since the HAL code works in STM32CubeIDE, there are unlikely to be issues with it.
Once that's determined, you can use that information to look for the part of the code that isn't doing the thing it's supposed to be doing.
In STM32CubeIDE this (examining peripheral register values) can be done via the SFRs window (Window -> Show View ->SFRs).
2024-01-03 8:57 PM
Thanks. I have tried to read out the registers, with (for example)
Note that the problem is not manifesting within STM32CubeIDE - my SPI test works fine there and as mentioned previously, I can communicate with the LCD. I'm trying to get the SPI working under PlatformIO - as above - the code worked fine with the F410, but doesn't work with the F412.
@TDK wrote:In STM32CubeIDE this (examining peripheral register values) can be done via the SFRs window (Window -> Show View ->SFRs).
2024-01-04 6:56 AM - edited 2024-01-04 6:58 AM
> This always returns 0 on all registers.
Then likely the SPI clock is not enabled. This should be done before configuring it or accessing any of its registers.
__HAL_RCC_SPIx_CLK_ENABLE();
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.