2014-07-30 3:05 PM
Hello!
Setup:2 custom boards (1 that's similar to the Discovery F4 and one that's based on a PSoC 5LP) linked by RS-485 (SN65HVD75 transceivers, half duplex, single twisted pair). Data flow: the STM32F4 is the Master. It can send data to the PSoC and the PSoC can read it (no problem here). It can also request data from the slave. In that case, the STM32 will send a data request, configure its transceiver to listen to the bus and, after a fixed delay, the PSoC will send its answer (for now, 5 test bytes). The problem:when I change the transceiver from TX to RX there is a glitch on the output line. The line goes low for ~25ns. It seems to be detected as a start bit by the STM's USART1 peripheral. I receive 5 bytes, as expected, but they are not the right value. The first 4 have a constant value and the last one is different. Start and stop bits are being seen as data. Or at least that's what it looks like.Experiments:I've tried to disable the USART, disable the reception, change the pin to be a GPIO, etc... without any success. Right now the test setup that I have has a wire going from the PSoC's TX line straight to the STM's RX line. By bypassing the transceiver I can receive the 5 bytes I'm sending by interrupt.
Code:
USART1 MSP:
void HAL_USART_MspInit( USART_HandleTypeDef * husart)
{ if(husart-> Instance==USART1) { /* Peripheral clock enable */ __USART1_CLK_ENABLE(); __GPIOA_CLK_ENABLE(); /**USART1 GPIO Configuration PA9 ------> USART1_TX PA10 ------> USART1_RX */ GPIO_InitStruct. Pin = GPIO_PIN_9|GPIO_PIN_10; GPIO_InitStruct. Mode = GPIO_MODE_AF_PP; //GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct. Pull = GPIO_PULLUP; //Transceiver's R is Hi-Z when !RE=1 GPIO_InitStruct. Speed = GPIO_SPEED_FAST; GPIO_InitStruct. Alternate = GPIO_AF7_USART1; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); } [...]USART1 Init function:
//USART1 init function: RS-485 #1
// Ref:http://eliaselectronics.com/stm32f4-tutorials/stm32f4-usart-tutorial/and Cube functions void USART1_Init( void ) { husart1. Instance = USART1; //MSP Init (enables clock, GPIOs) HAL_USART_MspInit(&husart1); //Interrupts: HAL_NVIC_SetPriority( USART1_IRQn, 0, 1); HAL_NVIC_EnableIRQ( USART1_IRQn); //UART1 module: //husart1.Init.BaudRate = 115200; husart1. Init. BaudRate = 921600; husart1. Init. WordLength = USART_WORDLENGTH_8B; husart1. Init. StopBits = USART_STOPBITS_1; husart1. Init. Parity = USART_PARITY_NONE; husart1. Init. Mode = USART_MODE_TX_RX; HAL_USART_Init(&husart1); //With only HAL_USART_Init() I never get an interrupt. Manually setting 5 bits: USART1-> CR1 |= 0b00000000000000010000000000100100; //16x oversampling , Receive enable, enable RXNE interrupts USART1-> CR2 &= 0b11111111111111111111011111111111; //Disable synchronous clock USART1-> CR3 &= 0b11111111111111111111011111111111; //3 bits method }This is what I call after I send a Reply Request. The request is as simple as
''
HAL_USART_Transmit
(&husart1,str,length,5000);''
//Prepares the board for a Reply (reception). Blocking.
unsigned char getc_rs485_1_blocking (void ) { unsigned int delay = 0; unsigned int tmp = 0; //Do not enable if still transmitting: while (husart1.State == HAL_USART_STATE_BUSY_TX); for (delay = 0; delay < 1000; delay++); //Short delay
//Receive enable rs485_set_mode(RS485_RX); for ( delay=
0; delay < 5000; delay++); //Short delay
tmp=
USART1-> DR; //Read buffer to clear
//Debug signal: HAL_GPIO_WritePin(GPIOF, GPIO_PIN_0, 1); HAL_GPIO_WritePin(GPIOF, GPIO_PIN_0, 0); return 0; }ISR (fires 5 times, once per byte):
void USART1_IRQHandler( void )
{ uint32_t tmp1 = 0, tmp2 = 0; unsigned int tmp = 0; //Rising edge, end of reception HAL_GPIO_WritePin(GPIOF, GPIO_PIN_0, 1); HAL_GPIO_WritePin(GPIOF, GPIO_PIN_0, 0); tmp1 = __HAL_USART_GET_FLAG(&husart1, USART_FLAG_RXNE); if (tmp1) { tmp = USART1-> DR; log_rx_bytes[cnt] = tmp; cnt++; if (cnt >= 20) cnt = 0; } HAL_USART_IRQHandler(&husart1); }As you can see in the code I've tried to use the 16x oversampling and the 3 bits averaging to filter out that glitch. It didn't change anything.
I'm obviously doing something wrong here. Can you spot my mistake?
Thanks!
2014-07-31 2:13 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.