2016-01-09 10:57 PM
2016-01-10 4:14 AM
Hi friend,
I have a same project with you. However, i use stm32f4 and ov7670, i use code of wareshare too and i have a problem like you when i try to send image data to PC. When i use DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&frame_buffer; DCMI seem not run, and i don't see anything in DCMI->DR. And other problem is i can't send data to usart when DCMI_Cmd(ENABLE); Are you finish, can you check whether it can send data usart while DCMI enable2016-01-10 6:29 AM
Probably want to think about the USART output routines, sending one character is not a string output function.
2016-01-10 5:08 PM
2016-01-24 2:36 AM
@clivel
Actually, I sent like this. Can this code be possible to send the frame?
printf(''%d \n'',Buffervalue(K+1));
printf(''%d \n'',Buffervalue(K+3));
if((K+1)%40==0)
printf(''; \r\n'');
And I also found the other problem which is when you see the DMA interruput part, there is the code that change frame_flag=1;
Actually, It changed well (I did debug by using printf function). However, In the while loop in main function. It wasn't changed.
I set the frame_flag as volatile int frame_flag as an global variable. any ideas could you give me?
Thank you
2016-01-24 6:04 AM
Ok, and if you stop it in a debugger does it provide any insight into where exactly it is stuck, or that the variable has changed? Can you look at and review the generated assembler code to see why that might not be working?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.