2013-06-23 8:11 PM
Hello, guys
I'm working on a stm32f407 chip and I wanna implement the I2C communication with it. But I have encountered some problems.The following describes my configuration about I2C:Enable clock for GPIOB and I2C.Remap I2C1 port to PB6, PB7PB6, 7 are configured in AF mode, open-drain, 50MHz output speed.I2C clock input is equal to APB1: 42MHzI2C_InitStruct.I2C_Mode = I2C_Mode_I2C;I2C_InitStruct.I2C_DutyCycle = I2C_DutyCycle_2;I2C_InitStruct.I2C_OwnAddress1 = 0x0A; //Master addressI2C_InitStruct.I2C_Ack = I2C_Ack_Enable; I2C_InitStruct.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; //7 bit address modeI2C_InitStruct.I2C_ClockSpeed = 100000; // speed = 300KAt last, the I2C peripheral is enabled.After these configuration, I was able to generate a start condition, and the status register is right.However, when I was trying to send the 7-bit slave address with bit0=0 (indicating a write operation according to EEPROM manual), the two status register value is 0x00070080. Only the BUSY, MSL, TRA,TxE bits are set. The ADDR bit is still keeping as 0.I don't know why the ADDR keeps reset, when the status of AF and TxE is right. I think a rights status of AF and TxE means a successful sending of address. Then what's wrong with the ADDR bit?Will anybody give me some advice about the possible reason for it? I have been stuck here for several days.Thank you!Wenlong Li #stm32 #i2c #cm4 #addr-bit2013-06-24 12:02 PM
You can try to perform software I2C reset before configuring I2C.
I had somewhat similar problem with STM32F1 but it couldn't always generate start condition, sometimes it worked and sometimes not, weird.Then I added software I2C reset and now it works flawlessly.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.