2015-11-24 8:32 PM
Hi ,
I'm using
a
STM32F405,my purpose is to receive the remote frame .but FIFO0 is not to receive the message . Namely , the function ''CAN2_RX0_IRQHandler'' interrupter is not access.
My CONFIG is:
hcan2.Init.Mode = CAN_MODE_NORMAL; hcan2.Init.SJW = CAN_SJW_1TQ; hcan2.Init.BS1 = CAN_BS1_3TQ; hcan2.Init.BS2 = CAN_BS2_2TQ; hcan2.Init.TTCM = DISABLE; hcan2.Init.ABOM = DISABLE; hcan2.Init.AWUM = DISABLE; hcan2.Init.NART = DISABLE; hcan2.Init.RFLM = DISABLE; hcan2.Init.TXFP = DISABLE;My Filter setup is:
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK; sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT; sFilterConfig.FilterIdHigh = 0x0000; sFilterConfig.FilterIdLow = 0x0000; sFilterConfig.FilterMaskIdHigh = 0x0000; sFilterConfig.FilterMaskIdLow = 0x0000; sFilterConfig.FilterFIFOAssignment = 0; sFilterConfig.FilterActivation = ENABLE; Can someone help to solve the question ,thank you all. #stm32-can-remoteWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.