2014-09-08 5:35 AM
Hi! I have a problem with MCO output (pin PC6) on STM32F405RG. I configured it with STM32CubeMX to generate about 36 MHz but I see only 8.97 MHz. How should I calculate correctPLLI2SN andPLLI2SR to get 36 MHz?
https://copy.com/MRClPwP0vLq3yqiI
void
SystemClock_Config(
void
) {
RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct;
RCC_OscInitTypeDef RCC_OscInitStruct;
__PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG( PWR_REGULATOR_VOLTAGE_SCALE1 );
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = 6;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 16;
RCC_OscInitStruct.PLL.PLLN = 336;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 4;
HAL_RCC_OscConfig( &RCC_OscInitStruct );
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
HAL_RCC_ClockConfig( &RCC_ClkInitStruct, FLASH_LATENCY_5 );
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_I2S;
PeriphClkInitStruct.PLLI2S.PLLI2SN = 258;
// 258
PeriphClkInitStruct.PLLI2S.PLLI2SR = 7;
HAL_RCCEx_PeriphCLKConfig( &PeriphClkInitStruct );
}
#stm32f4 #mco
2014-09-08 8:09 AM
Yeah, well PLLIS2 isn't going to come out of MCO1 (PA8), at least according to RM0090
You could get 33.6 MHz out using 168 MHz DIV5 Your inquiry with respect to HAL code might be better served on the other forum. I don't see any code here configuring the MCO pin(s), or how 36 MHz would come out based on the settings. PC6 is I2S2_MCK, PC9 is MCO22014-09-09 2:04 AM
Oh, sorry! Of course I meant I2S2_MCK (before posting I read many threads on this forum and mixed pin name). So, according to settings in STM32CubeMX I should get on I2S2_MCK (PC6) 857 MHz, but I get 8.97 MHz. STM32CubeMXconfigured PLLI2S like this:
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_I2S;
PeriphClkInitStruct.PLLI2S.PLLI2SN = 258;
PeriphClkInitStruct.PLLI2S.PLLI2SR = 7;
HAL_RCCEx_PeriphCLKConfig( &PeriphClkInitStruct );
What could be the reason?
2014-09-09 9:22 AM
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2014-09-10 4:03 AM
Thank you very much, it works!
It would be good to see warning in STM32 software that I could not get this frequency on PC6 pin.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.