2015-11-26 4:54 AM
Hello everybody!
I'm trying to configure the main PLL to generate the max clock frequency (84 MHz on this board), and I'm using the HSI as PLL source.I made some test:- test1: HCLK=70 MHzM=16N=140P=2AHB_PR=1APB1_PR=2APB2_PR=1As soon as I set the PLL output as HCLK, the uC stops working.I mean:- no blinking led- random value on general purpose registerI made some test:- test2: HCLK=35 MHzM=16N=140P=2AHB_PR=2APB1_PR=2APB2_PR=1The uC works normally.I'm missing some configuration (i.e. ART?), or the problem is the HSI and his accuracy?Could someone help me to figure it out? Thanks!Regards2015-11-26 5:17 AM
Set FLASH latency properly.
JW2015-11-26 5:32 AM
You also seem to be running the VCO very slowly. Doesn't it specify 192 - 432 MHz
For 84 MHz, ST runs the VCO/PLL at 336 MHz and divides that by 4 (N)2015-11-26 5:51 AM
I did not check for 'F401 specifically, but doesn't the reviewed PLL range apply for them too?
https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/DispForm.aspx?ID=59917 JW2015-11-26 6:47 AM
Thanks both of you for your input!
Regads2015-11-26 10:10 AM
From the RM i read this:
1. Program the new number of wait states to the LATENCY bits in the FLASH_ACRregister
2. Check that the new number of wait states is taken into account to access the Flash
memory by reading the FLASH_ACR register
3. Modify the CPU clock source by writing the SW bits in the RCC_CFGR register
4. If needed, modify the CPU clock prescaler by writing the HPRE bits in RCC_CFGR
5. Check that the new CPU clock source or/and the new CPU clock prescaler value is/are
taken into account by reading the clock source status (SWS bits) or/and the AHB
prescaler value (HPRE bits), respectively, in the RCC_CFGR register
To achieve point 2 and 5 I used the istruction DSB and ISB. Is it right, or I need to check the state of bits?************************************************************************************************************ ; Set PLL at 70 MHz and use his output as clock sys LDR r0, =0x40023800 ; RCC ldr r1, =0x27015410 ; M=16, N=336, P=4, Q=7, HSI source PLL str r1, [r0, #0x4] ; PLLCFGR ldr r1, [r0] ; RCC_CR orr r1, r1, #(1 << 24) ; PLLON=1 str r1, [r0] ; wait states for FLASH ldr r2, =0x40023C00 ; FLASH register ldr r3, =0x302 ldr r1, [r2] ; FLASH_ACR orr r1, r1, r3 ; ICEN=1, PRFTEN=1, 2 WS= 60<HCLK<=84 str r1, [r2] DSB ISB ldr r1, =0x1002 str r1, [r0, #0x8] ; PLL as clock sys, AHB_PR=1, APB1_PR=2, APB2_PR=1 DSB ISB***********************************************************************************************************RegardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.