2015-01-18 3:11 AM
Hello.
I am use example VCP from the ST. on STM32f405I am working under WinXP with a virtual COM port via the API as a file.Cyclically sends data (short packets from 8 to 16 bytes) from PC to Device by function - WriteFile.Data transfer immediately, but from time to time there is a strange TimeOut to transfer (WriteFile) sometimes up to 500ms.Same work, but with a real COM port, such delays are not present.What could be the problem?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.