2014-10-02 10:55 AM
Hi everyone,
So i wanted to get into ST ARMs microcontrolers. I only used TI Tivas before but i wanted to try out the ST ones.Well i would like to know if anyone could provide some links to tutorials and such. My main problem is the compiler. I can't seem to start a project in IAR workbench.If anyone also has suggestions for other compilers i would appreciate it2014-10-02 11:01 AM
Most IDE's function in materially similar ways, I'd suggest you look at the Examples and project templates included with the Standard Peripheral Libraries. Understand the construction of those, the library files pulled in, the include paths, and compiler defines.
This covers the STM32F1, but might provide additional insighthttp://www.cs.indiana.edu/~geobrown/book.pdf
2014-10-02 11:06 AM
Sincerely i spent hours trying to get a code to work. I use Cube examples and i was fine but i couldn't create a new project not even from a existing one nor the templates. A bit discouraging. I tried copying, editing, adapting the options and paths but nothing
I don't understand, i use IAR for the Tiva and i only take less than 2min now, it can't be that hard with the STM32.2014-10-03 1:56 AM
Here is my quick start VIDEO how to set up STM32F4 in IAR IDE
https://www.youtube.com/watch?v=FV5x-RiyKqo&list=UUDBSFAz0IZN4Jjs07bH1XqQ2014-10-03 5:11 AM
Thanks, i will check it out later more in depth but it seems exactly what i need
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.