2022-08-01 9:39 PM
hi,
i'm trying to read the external adc value using spi1 + dma (MAX11198ATE+)
i though it works fine but, sometimes it returns wrong values
i have checked the waveforms of SPI MISO/MOSI, SCK (hardware)
but there was no error forms. it seems to be matched in timing chart
@@
i have checked spi mode and tested this for TI mode (hardware output NSS) and motorola mode (in this case, NSS was not Used)
but result was same
@@
there was no effect for changing the compile optimization level 0 ~ 3
when i debugging the firmware source, rx buffer for spi dma is below
(1)
desiable return value range : 0xD2E0 ~ 0x D310
(2)
wrong value : 0xD200 or D3FE~F
you can see the below image
look at the buffer index [1] / [20]
it seems to be fluctuated (low byte units or middle 1 bits)
i don't know what happens
i just called hal libray for reading value using spi..
there was no custom library..
and i have read the m4 reference manual many times
but i don't undertand..
here is my initial setting code on spi dma
first,
i have set the main system clock '128MHz' and APB2 '64MHz' due to spi1 sck clock for 32MHz
second,
spi + tx / rx dma settings with circular mode
//------------------------------------------------------------------------------------
/* SPI1 DMA Init */
/* SPI1_RX First Init Befor Tx Init */
hdma_spi1_rx.Instance = DMA2_Stream0;
hdma_spi1_rx.Init.Channel = DMA_CHANNEL_3;
hdma_spi1_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_spi1_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi1_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi1_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
hdma_spi1_rx.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
hdma_spi1_rx.Init.Mode = DMA_CIRCULAR;
hdma_spi1_rx.Init.Priority = DMA_PRIORITY_VERY_HIGH;
hdma_spi1_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
if (HAL_DMA_Init(&hdma_spi1_rx) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(spiHandle, hdmarx, hdma_spi1_rx);
/* SPI1_TX Init */
hdma_spi1_tx.Instance = DMA2_Stream3;
hdma_spi1_tx.Init.Channel = DMA_CHANNEL_3;
hdma_spi1_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_spi1_tx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi1_tx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi1_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
hdma_spi1_tx.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
hdma_spi1_tx.Init.Mode = DMA_CIRCULAR;
hdma_spi1_tx.Init.Priority = DMA_PRIORITY_VERY_HIGH;
hdma_spi1_tx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
if (HAL_DMA_Init(&hdma_spi1_tx) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(spiHandle, hdmatx, hdma_spi1_tx);
/* SPI1 interrupt Init */
HAL_NVIC_SetPriority(SPI1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(SPI1_IRQn);
//------------------------------------------------------------------------------------
after the code periperal is set, i called
hal_spi_transmitreceive_dma(...)
also, either dma fifor setting enable or not was not affected in the result
anyone help
thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.