2013-02-25 4:13 PM
HI ST COMMUNITY,
I just wondering why my stm32f4 Discovery board seems to slowed down, I am still using the same program. I've just powered it on as usual and make it do its usual task of capturing data.. Then when I try to see the data it is capturing it is incomplete so I tried to re program it... still same results so I tried to see the signals on the scope and yes it really have slowed down so I have decreased the delay but now It cannot decode numeric data properly. I will still check if the cable is the problem. but before that happened I am usually using it to transfer captured data on the serial at 961200 at a delay of FFF the program that recieves the data is a labview program. I have used a delay of FFF because the program cannot see data at a delay of FF now it can read at a delay of FF and if i increas my delay to FFF suceeding data are not read2013-02-25 4:17 PM
2013-02-25 5:06 PM
Corrupt data is more of a sign of signal noise than silicon bit rot. Perhaps you have a bad ground connection, supply issues for the PLL/VCO, or you need to slow the data transfer down to more realistic levels. Asynchronous serial is not considered very robust.
Consider what you have changed, cables you connected, etc.2013-02-25 6:19 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.