2018-10-19 5:40 AM
Does anyone already have been generate three sine wave using stm32f4?
Solved! Go to Solution.
2018-10-19 7:36 AM
Only has two DACs
2018-10-19 7:36 AM
Only has two DACs
2018-10-19 1:40 PM
use an external Quad DAC,
the easiest interface I ever did
only took 10 minutes before it worked.
2018-10-19 1:40 PM
use an external Quad DAC,
the easiest interface I ever did
only took 10 minutes before it worked.
2018-10-19 1:40 PM
use an external Quad DAC,
the easiest interface I ever did
only took 10 minutes before it worked.
2018-10-19 5:59 PM
Thank you. But as I understand your answers, we just could generate TWO sine wave with TWO DACs? I need THREE sine wave for control 3 phase AC motor.
2018-10-20 1:28 PM
what speed do you need in RPM ?
You need 3 Dacs for 3 sinewaves...
2018-10-20 6:16 PM
Thank you for your reply. I need about 3000rpm. So can I use 3 DACs for generate sinewave? In addition, can I generate 3 sinewave use DACs with PHASE SHIFT (120 degrees).
2018-10-20 7:35 PM
Yes of course.
so you need a Sine wave in Flash, and feed it to the DAC at the right time
if your sine wave hast 8 steps, ( which is not much of a sine wave)
how many poles does the motor have ?
3000 x 60 x Poles x 8 points(in Sinewave)
guessing 2 or 3 poles...
that's a feed rate of 2.8MHz per channel... if you want 16 bit, double that.
that is going to be difficult for a veteran.
This seems a stretch from being practicable.
there are other methods of driving motors, maybe some more research is needed.
2018-10-20 10:25 PM
Thank you TJ. Your information really useful for me. And yes, there's difference method of driving AC motors, but I want to practice the simple method, is Vf control or Scalar control. I already have been made that with dsp kit of TI, but for ARM, the problem is I don't know how to generate 3 phase sine wave. That's why I post it to this forum.
Again thank you for your share.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.