2013-06-02 4:34 AM
hello :)
i had a problem when i send a character or receive a character , i always get a wrong character like ''-'' or a heart ... ps: i'm using rs232 -> USB converter here is my code: &sharpinclude ''stm32f4xx.h'' void main() { //UART4 initialization RCC->APB1ENR |= 0x00080000; // Enable clock for UART4 RCC->AHB1ENR |= 0x00000004; // Enable clock for GPIOC GPIOC->MODER |= 0x00a00000; // PC10, PC11 => AF mode GPIOC->AFR[1] |= 0x00008800; // select AF8 (UART4,5,6) for PA10, PA11 UART4->BRR = 0x1120; // 9600 baud UART4->CR1 |= 0x200c; // Enable UART for TX, RX UART4->CR1 |= 0x0020; // Enable RX interrupt while(1){ if (UART4->SR & 0x0080) { UART4->DR='a'; for (int i=0; i<10000000; i++) {}; } } } please any help! :( #too-vague2013-06-02 7:23 AM
please any help!
With register level code you really own your own problems. The baud rate value looks wrong, For a chip running at 168 MHz, and APB1 at 42 MHz, 0x1117 would be better for actually getting 9600 baud. Why would you enable a receive interrupt?// STM32 UART4 (Tx PC.10, Rx PC.11) STM32F4 Discovery - sourcer32@gmail.com
// PC11 technically conflicts with SCLK on CS43L22
#include ''stm32f4_discovery.h''
/**************************************************************************************/
void RCC_Configuration(void)
{
/* --------------------------- System Clocks Configuration -----------------*/
/* UART4 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_UART4, ENABLE);
/* GPIOC clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/*-------------------------- GPIO Configuration ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOC, &GPIO_InitStructure);
/* Connect USART pins to AF */
GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_UART4);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_UART4);
}
/**************************************************************************************/
void UART4_Configuration(void)
{
USART_InitTypeDef USART_InitStructure;
/* USARTx configuration ------------------------------------------------------*/
/* USARTx configured as follow:
- BaudRate = 115200 baud
- Word Length = 8 Bits
- One Stop Bit
- No parity
- Hardware flow control disabled (RTS and CTS signals)
- Receive and transmit enabled
*/
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(UART4, &USART_InitStructure);
USART_Cmd(UART4, ENABLE);
}
/**************************************************************************************/
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
UART4_Configuration();
while(1)
{
while(USART_GetFlagStatus(UART4, USART_FLAG_TXE) == RESET); // Wait for Empty
USART_SendData(UART4, 0x49); // Send 'I'
}
while(1); // Don't want to exit
}
2013-06-02 12:17 PM
thnx for your reply! :)
but it still didnt work for me :\ even i changed the baud rate to many values2013-06-02 7:41 PM
In that case you'll need to pay particular attention to the crystal on the board, the define for HSE_VALUE, and the PLL settings in system_stm32f4xx.c. Most notably, the STM32F4-Discovery board uses an 8 MHz crystal, and most of ST's other offerings use a 25 MHz crystal. Failing to deal with this will result in baud rates being wrong, I highly recommend sending characters repetitively and measuring the bit time with a scope.
2013-06-03 2:30 PM
thnx clive for urr answer :) this is my config in system_stm32f4xx.c and plz tell me what can i do
This file configures the system clock as follows: *============================================================================= *============================================================================= * Supported STM32F4xx device revision | Rev A *----------------------------------------------------------------------------- * System Clock source | PLL (HSE) *----------------------------------------------------------------------------- * SYSCLK(Hz) | 168000000 *----------------------------------------------------------------------------- * HCLK(Hz) | 168000000 *----------------------------------------------------------------------------- * AHB Prescaler | 1 *----------------------------------------------------------------------------- * APB1 Prescaler | 4 *----------------------------------------------------------------------------- * APB2 Prescaler | 2 *----------------------------------------------------------------------------- * HSE Frequency(Hz) | 25000000 *----------------------------------------------------------------------------- * PLL_M | 25 *----------------------------------------------------------------------------- * PLL_N | 336 *----------------------------------------------------------------------------- * PLL_P | 2 *----------------------------------------------------------------------------- * PLL_Q | 7 *----------------------------------------------------------------------------- * PLLI2S_N | NA *----------------------------------------------------------------------------- * PLLI2S_R | NA *----------------------------------------------------------------------------- * I2S input clock | NA *----------------------------------------------------------------------------- * VDD(V) | 3.3 *----------------------------------------------------------------------------- * Main regulator output voltage | Scale1 mode *----------------------------------------------------------------------------- * Flash Latency(WS) | 5 *----------------------------------------------------------------------------- * Prefetch Buffer | OFF *----------------------------------------------------------------------------- * Instruction cache | ON *----------------------------------------------------------------------------- * Data cache | ON *----------------------------------------------------------------------------- * Require 48MHz for USB OTG FS, | Enabled * SDIO and RNG clock | *-----------------------------------------------------------------------------2013-06-03 3:07 PM
Do you have an STM32F4-Discovery board? I've kind of assumed this, but you've not explicitly stated what you're using.
If so you'll need to modify the PLL_M define to 8 in this file, and define HSE_VALUE as 8000000 within the project. In Keil it would be Options -> C/C++ -> Preprocessor Symbols -> Define Should be something like : STM32F4XX, USE_STDPERIPH_DRIVER, HSE_VALUE=8000000 For IAR you'll need to read your manuals. Make sure it's not redefined in any other source files.2013-06-04 4:08 AM
thnx! i think i'm near to the good results , because it changed a little and the characters are better but still wrong , i changed the PLL_M to 8 and HSE to 8Mhz , i think it still something missing :)
should i change also the APB1 Prescaler or no ? and what is the new baud rate value i should put it ?2013-06-04 4:09 AM
and yeah i'm using STM32F4
2013-06-04 4:34 AM
Have you checked the bit timing with a scope?
Why would you need to change the APB settings? The PLL value being changed is the one that generates the 1 MHz comparison frequency internally. The other setting should get us to 168 MHz. The startup_stm32f4xx.s code calls the SystemInit() routine in system_stm32f4xx.c, and it is this code that should set up the pll and buses. You could also use timers, and MCO pins to confirm internal clock speeds with a scope.2013-06-04 11:29 AM
anyway i dont have scope to test on it , i'm little confused what to do
thnx anyway clive :)We’re moving the ST Community to a new platform to give you a better and more reliable community experience.