2018-07-10 6:42 AM
Hello,
I have a problem with the pins PB8 and PB9 as GPIO. I habe used the following testcode on the EVAL324xG-EVAL Board:
int main () {
GPIO_InitTypeDef GPIO_InitStructure;
RCC_AHB1PeriphClockCmd (RCC_AHB1Periph_GPIOB, ENABLE); GPIO_InitStructure.GPIO_Pin = (GPIO_Pin_8 | GPIO_Pin_9); GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_OD; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init (GPIOB, &GPIO_InitStructure);GPIO_SetBits(GPIOB, GPIO_Pin_8);
GPIO_SetBits(GPIOB, GPIO_Pin_9); while (1);}
Both pins drive the voltage.
On the pin PB8 drives the voltage to ground. When I connect a 2k2 pullup resistor on pin PB8, then the voltage is 2.2V.
On the pin PB9 drives the voltage to vdd. When I connect a 2k2 pulldown resistor on pin PB9, then the voltage is 1.6V.
If the MCU is in the reset state (input mode is activated), I have the same problem. I don't understand this effect.
When I configure the output type as a push-pull instead of open drain, then the MCU drives as expected the pins.
Thanks for your help!
#gpio #stm32f42018-07-10 7:04 AM
Any other circuitry connected to those pins?
Any other code running?
Read out and check/post the relevant GPIO registers' content.
JW
2018-07-10 11:08 PM
I am trying to program the I2C1 interface on these pins. Of course the GPIO_Mode must be at GPIO_Mode_AF. But I have with the I2C configuration the same problem. The I2C3 with the pins PA8 and PC9 is running.
I thought maybe the EVAL-Board is defective. But the STM32F4 discovery Board also drives pin PB9 in the reset state to vdd.
The register values of GPIOB by upper code are:
MODER = 0x0005 0280 (MODER9 = 0x1; MODER8 = 0x1)
OTYPER = 0x0000 0300 (OT9 = 0x1; OT8 = 0x1)
OSPEEDR = 0x000a 00c0 (OSPEEDR9 = 0x2; OSPEEDR8 = 0x2)
PUPDR = 0x0000 0100 (PUPDR9 = 0x0; PUPDR8 = 0x0)
IDR = 0x0000 c350 (IDR9 = 0x1; IDR8 = 0x1)
ODR = 0x0000 0300 (ODR9 = 0x1; ODR8 = 0x1)
LCKR = 0x0000 0000 (LCK9 = 0x0; LCK8 = 0x0)
AFRL = 0x0000 0000 (AFRL9 = 0x0; AFRL8 = 0x0)
AFRH = 0x0000 0000 (AFRH9 = 0x0; AFRH8 = 0x0)
I mean a other function of this pins are have a higer priority as the GPIO, but I haven't found any.
Thanks for your help!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.