2012-02-21 1:16 PM
In the reference manual (section 26.1) it says:
The SDIO features include the following:? Full compliance with MultiMediaCard System Specification Version 4.2.
Card support for three different databus modes: 1-bit (default), 4-bit and 8-bitbut later, in Note 2, we see the odd sentence:The current version of the SDIO supports only one SD/SDIO/MMC4.2 card at any one time and a stack of MMC4.1 or previous.
Why does it specify ''a stack of MMC4.1 or previous''?There were some major changes between the MMC4.1 and MMC4.2 specifications; one very important one was that 4.2 added the ability to specify addresses using 32-bit sector numbers instead of 32-bit byte addresses.Can someone explain how the SDIO is fully compliant with the MMC spec 4.2 but not with an MMC 4.2 stack?Thanks... #stm32f4-mmc
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.