2014-03-20 8:29 AM
Hi, I'm still start in STM32F4 I am looking for how to use the ADC interrupt that will allow me to read sensor values and the interruption with TIM that will allow me to read the values back by an encoder
2014-03-20 8:54 AM
Review Example code provided in the Firmware Libraries
STM32F4-Discovery_FW_V1.1.0\Project\Peripheral_Examples\TIM_TimeBase STM32F4xx_DSP_StdPeriph_Lib_V1.3.0\Project\STM32F4xx_StdPeriph_Examples\TIM\TIM_TimeBase There are also several ADC examples, perhaps not generating EOC interrupts. And I've posted a lot of examples on the forum, though I'd recommend Google over the board search2014-03-20 9:07 AM
Hi thank you for your reply, I want a trick to run the fontion ''readsensor'' in parallel with (while (1))
int main(void){ ADC1_CH12_DMA_Config(); ADC_SoftwareStartConv(ADC1); readsensor(); while (1) { if (val[0]>4000) {GPIO_SetBits(GPIOD, GPIO_Pin_12); }else {GPIO_ResetBits(GPIOD, GPIO_Pin_12);} }}2014-03-20 9:28 AM
Configure the DMA to interrupt at HT/TC events.
Not sure what DMA/Channel/Stream you're using. Enable the NVIC, Enable IRQ on DMA, create IRQHandler()[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/3%20channels%20on%20ADC1%20and%20DMA&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=504]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2F3%20channels%20on%20ADC1%20and%20DMA&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=5042014-03-20 3:58 PM
void NVIC_Configuration(void) {
NVIC_InitTypeDef NVIC_InitStructure; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; /* Enable DMA1 channel1 IRQ Channel */ NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel1_IRQn; NVIC_Init(&NVIC_InitStructure);}er : ..\main.c(589): error: #20: identifier ''DMA1_Channel1_IRQn'' is undefined2014-03-20 4:15 PM
er : ..\main.c(589): error: #20: identifier ''DMA1_Channel1_IRQn'' is undefined
Yeah, because that's not how it's done, I'll play this game but you'll need to post complete code, not out of context fragments. DMA1_Stream1_IRQn ?2014-03-20 7:51 PM
Example of single channel ADC using EOC interrupt
2014-03-20 8:24 PM
// STM32F4-Discovery ADC1 3CH DMA IRQ - sourcer32@gmail.com
#include ''stm32f4_discovery.h''
//******************************************************************************
#define SAMPLES (3 * 2) // 3 SAMPLES, TWICE
volatile uint16_t ADCConvertedValues[SAMPLES];
//******************************************************************************
void NVIC_Configuration(void)
{
NVIC_InitTypeDef NVIC_InitStructure;
/* Enable the ADC1 gloabal Interrupt */
NVIC_InitStructure.NVIC_IRQChannel = DMA2_Stream0_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
}
//******************************************************************************
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB | RCC_AHB1Periph_GPIOC, ENABLE);
/* Configure ADC1 Channel8 pin as analog input PB0 */
/* Configure ADC1 Channel9 pin as analog input PB1 */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(GPIOB, &GPIO_InitStructure);
/* Configure ADC1 Channel12 pin as analog input PC2 */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2;
GPIO_Init(GPIOC, &GPIO_InitStructure);
}
//******************************************************************************
void ADC1_Configuration(void)
{
ADC_InitTypeDef ADC_InitStructure;
ADC_CommonInitTypeDef ADC_CommonInitStructure;
DMA_InitTypeDef DMA_InitStructure;
/* Enable peripheral clocks */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
/* DMA2_Stream0 channel0 configuration */
DMA_DeInit(DMA2_Stream0);
DMA_InitStructure.DMA_Channel = DMA_Channel_0;
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&ADC1->DR;
DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&ADCConvertedValues[0];
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;
DMA_InitStructure.DMA_BufferSize = SAMPLES;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;
DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;
DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
DMA_Init(DMA2_Stream0, &DMA_InitStructure);
/* DMA2_Stream0 enable */
DMA_Cmd(DMA2_Stream0, ENABLE);
/* Enable DMA Stream Half Transfer and Transfer Complete interrupts */
DMA_ITConfig(DMA2_Stream0, DMA_IT_HT, ENABLE);
DMA_ITConfig(DMA2_Stream0, DMA_IT_TC, ENABLE);
/* ADC Common Init */
ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;
ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;
ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;
ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;
ADC_CommonInit(&ADC_CommonInitStructure);
/* ADC1 Init */
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ScanConvMode = ENABLE; // Multiple Channels
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; // Keep Sampling
ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfConversion = 3;
ADC_Init(ADC1, &ADC_InitStructure);
/* ADC1 regular channel configuration ******************************/
ADC_RegularChannelConfig(ADC1, ADC_Channel_8, 1, ADC_SampleTime_480Cycles); // PB0
ADC_RegularChannelConfig(ADC1, ADC_Channel_9, 2, ADC_SampleTime_480Cycles); // PB1
ADC_RegularChannelConfig(ADC1, ADC_Channel_12, 3, ADC_SampleTime_480Cycles); // PC2 (BANKC)
/* Enable DMA request after last transfer (Single-ADC mode) */
ADC_DMARequestAfterLastTransferCmd(ADC1, ENABLE);
/* Enable ADC1 DMA */
ADC_DMACmd(ADC1, ENABLE);
/* Enable ADC1 */
ADC_Cmd(ADC1, ENABLE);
/* Start ADC1 Software Conversion */
ADC_SoftwareStartConv(ADC1);
}
//******************************************************************************
void DMA2_Stream0_IRQHandler(void)
{
/* Test on DMA Stream Half Transfer interrupt */
if (DMA_GetITStatus(DMA2_Stream0, DMA_IT_HTIF0))
{
static int i = 0;
/* Clear DMA Stream Half Transfer interrupt pending bit */
DMA_ClearITPendingBit(DMA2_Stream0, DMA_IT_HTIF0);
/* Toggle LED3 */
if ((i++ % 1000) == 0)
STM_EVAL_LEDToggle(LED3); /* Toggle Red LED */
/* Add code to process First Half of Buffer */
}
/* Test on DMA Stream Transfer Complete interrupt */
if (DMA_GetITStatus(DMA2_Stream0, DMA_IT_TCIF0))
{
static int i = 0;
/* Clear DMA Stream Transfer Complete interrupt pending bit */
DMA_ClearITPendingBit(DMA2_Stream0, DMA_IT_TCIF0);
/* Toggle LED4 */
if ((i++ % 1000) == 0)
STM_EVAL_LEDToggle(LED4); /* Toggle Green LED */
/* Add code to process Second Half of Buffer */
}
}
//******************************************************************************
int main(void)
{
GPIO_Configuration();
STM_EVAL_LEDInit(LED3); // Red
STM_EVAL_LEDOn(LED3);
STM_EVAL_LEDInit(LED4); // Green
STM_EVAL_LEDOff(LED4);
NVIC_Configuration();
ADC1_Configuration();
while(1); /* Infinite loop */
}
/**************************************************************************/
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* User can add his own implementation to report the file name and line number,
ex: printf(''Wrong parameters value: file %s on line %d
'', file, line) */
while (1)
{}
}
#endif
/**************************************************************************/
2014-03-22 9:39 AM
2014-03-22 6:10 PM
Ok, so you need to manage things in interrupt handlers, and a foreground while loop, OR you need to invest some time/effort investigating the use of an RTOS
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.