2016-10-03 2:36 AM
Hi,
I want to read the internal temperature of STM32F429II. I am using stm32F4 peripheral library V1.4.4. Below is my code,// Initstatic HAL_StatusTypeDef ADCx_Init(void){ hAdc.Instance = ADC1; if (HAL_ADC_DeInit(&hAdc) != HAL_OK) { return HAL_ERROR; } if (HAL_ADC_GetState(&hAdc) == HAL_ADC_STATE_RESET) { hAdc.Init.ClockPrescaler = ADC_Prescaler_Div2; hAdc.Init.Resolution = ADC_RESOLUTION_12B; hAdc.Init.DataAlign = ADC_DATAALIGN_RIGHT; hAdc.Init.ScanConvMode = DISABLE; hAdc.Init.EOCSelection = ADC_EOC_SINGLE_CONV; hAdc.Init.ContinuousConvMode = ENABLE; hAdc.Init.NbrOfConversion = 1; hAdc.Init.DiscontinuousConvMode = DISABLE; hAdc.Init.NbrOfDiscConversion = 1; hAdc.Init.ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1; hAdc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; hAdc.Init.DMAContinuousRequests = DISABLE; if (HAL_ADC_Init(&hAdc) != HAL_OK) { return HAL_ERROR; } hAdc_AdcChannelConfig.Channel = ADC_CHANNEL_TEMPSENSOR; hAdc_AdcChannelConfig.SamplingTime = ADC_SAMPLETIME_480CYCLES; hAdc_AdcChannelConfig.Rank = 1; hAdc_AdcChannelConfig.Offset = 0; if (HAL_ADC_ConfigChannel(&hAdc, &hAdc_AdcChannelConfig) != HAL_OK) { return HAL_ERROR; } } return HAL_OK;}//Clock// in stm32f4xx_hal_msp.cvoid HAL_ADC_MspInit(ADC_HandleTypeDef* hadc){ __HAL_RCC_ADC_CLK_ENABLE(); }// Call this function at some interval from main to read temperatureuint16_t sampleInput(void){ float TemperatureValue = 0; uint16_t value = 0; if (HAL_ADC_Start(&hAdc) != HAL_OK) { printf(''HAL_ADC_Start fail\r\n''); return HAL_ERROR; } if (HAL_ADC_PollForConversion(&hAdc, HAL_MAX_DELAY) != HAL_OK) { printf(''HAL_ADC_PollForConversion fail\r\n''); return HAL_ERROR; } if((HAL_ADC_GetState(&hAdc) & HAL_ADC_STATE_REG_EOC) != HAL_ADC_STATE_REG_EOC) { printf(''HAL_ADC_GetState fail\r\n''); return HAL_ERROR; } value = HAL_ADC_GetValue(&hAdc); printf(''HAL_ADC_GetValue [%x] [%d]\r\n'', value, value); TemperatureValue = value&0x0fff;// 12 bit result TemperatureValue *= 3300; TemperatureValue /= 0xfff; //Reading in mV TemperatureValue /= 1000.0; //Reading in Volts TemperatureValue -= 0.760; // Subtract the reference voltage at 25�C TemperatureValue /= .0025; // Divide by slope 2.5mV TemperatureValue += 25.0; // Add the 25�C printf(''Temp = [%f]\r\n'', TemperatureValue);}I am stuck here in ''HAL_ADC_PollForConversion'' function. Please help me out of this.
#adc #!stm32 #internal-temperature-sensor2016-10-03 3:03 AM
Hello,
I recommend to you using latest version of v1.13.0 firmware There is always enhancement and bug fixes in the new release.Regards2016-10-03 3:34 AM
__HAL_RCC_ADC_CLK_ENABLE.
Now, This code is working fine. Thanks!!!!!!!2019-03-04 3:42 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.